This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The C6Run tool does not use the Codec Engine framework. It provides a simplified mechanism to build and run C code from the ARM/Linux command prompt, with execution being handled transparently by the DSP core. The C6Run tools are not directly related to Codec Engine or the XDC tools.
I would encourage you to read the documentation available on the TI embedded processors wiki and post any further questions here.
Regards, Daniel
HI~ Daniel Allred !
Thank your reply and suggestion .
So user can use own Library *.h to make C code with c6run-tool too ?
Yes, the intention is that the user can supply their own C files and header files and compile them with the C6Run tools to run on the DSP. The programs are run from the ARM/Linux command prompt, but execution takes place on the DSP without the user having to know much about the communication that takes place between the two cores to make that happen.
There are two use cases right now. The C6RunApp case moves all of the user application code to the DSP, including the main() function. Any C I/O operations (such as printf, scanf, fopen, fread, etc) will be sent to the ARM and the results will then be returned to the DSP. The second use case, C6RunLib, allows the user to move only certain C files to the DSP by creating a separate library that is then linked in at build time with the remainder of the user's code which runs on the ARM. Any calls that are made into that library are then executed on the DSP and the results are returned to the ARM.
I hope the above description helps. Much more detail can be found on the TI embedded processor wiki.
Regards, Daniel