Hi All ,
We have usercase where we have to route all data packets (MAC and IP packets ) received in the Ethernet port to the either main2_1 or A72 cores. I see the current ethernet firmware (main2_0 ) has the default PHY configuration for DP83867ERGZT which is used in the EVM board. Have some below questions.
Quad Port Eth expande- EVM board
1. In the EVM, there is a expansion board Quad Port Eth expander which has four RJ45 connecor.
2.Are all connected to single port of mcu cpsw2 ?
3.Is any of these port is connected to main_cpsw9 ?.
4.Do we need to do any additional configuration either from ethfw or the client softwares to configure the same. If these four ports are muxed to single port ,how to select the connected one.
PC packet generator tools
1.We like to have packet generator tools both for generating raw packets (MAC) and tcp/ip packets. Can you share the link to the insallers where we get the tools installed in Linux.
Custom Eth Interfaces :
1. In our custom board we have 2 more interfaces connected RTL9010(PHY) and Marvel 88Q5050(Ext Switch) connected to CPSW9 ports. For configuring them which files should we have in Ethfw we need to modify.
Can ypu provide answers for the above questions?
With regards,
Jeyaseelan