Part Number: OMAP-L138
Hi,
I came across an issue in section 1.1.8. GCC ToolChain (link below) in the section at the very bottom Configure/Autotools:
http://software-dl.ti.com/processor-sdk-linux/esd/docs/latest/linux/Overview/GCC_ToolChain.html
The line ./configure –host=i686 –disable-deinterlace2 –disable-x264 has an issue where each – is not a -.
When I copied and pasted the line ./configure –host=i686 –disable-deinterlace2 –disable-x264 into my command line and executed it the output was:
configure: error: invalid variable name: –host
After some head scratching I modified ./configure –host=i686 –disable-deinterlace2 –disable-x264 to ./configure -host=i686 -disable-deinterlace2 -disable-x264 and the command was taken.
I hope this helps out anyone else in the same situation.
Ben