Part Number: AM5728
Hi,
We are using AM5728 in our custom boards. I am trying to compile (in my Ubuntu 14.04LTS machine) OpenCL projects located in <path-to-sdk-linux>/example-applications/opencl-examples-1.2.00.02
But I am getting the below errors.
=============== offline =================
Compiling main.cpp
main.cpp:29:10: fatal error: CL/cl.hpp: No such file or directory
#include <CL/cl.hpp>
^~~~~~~~~~~
compilation terminated.
../make.inc:238: recipe for target 'main.o' failed
make[1]: *** [main.o] Error 1
=============== simple =================
/home/user/Vijay_HS/UACE_2030/sdk-linux/linux-devkit/sysroots/x86_64-arago-linux/usr/bin/../lib/gcc/arm-linux-gnueabihf/8.3.0/../../../../arm-linux-gnueabihf/bin/ld: cannot find crt1.o: No such file or directory
/home/user/Vijay_HS/UACE_2030/sdk-linux/linux-devkit/sysroots/x86_64-arago-linux/usr/bin/../lib/gcc/arm-linux-gnueabihf/8.3.0/../../../../arm-linux-gnueabihf/bin/ld: cannot find crti.o: No such file or directory
/home/user/Vijay_HS/UACE_2030/sdk-linux/linux-devkit/sysroots/x86_64-arago-linux/usr/bin/../lib/gcc/arm-linux-gnueabihf/8.3.0/../../../../arm-linux-gnueabihf/bin/ld: cannot find -lOpenCL
/home/user/Vijay_HS/UACE_2030/sdk-linux/linux-devkit/sysroots/x86_64-arago-linux/usr/bin/../lib/gcc/arm-linux-gnueabihf/8.3.0/../../../../arm-linux-gnueabihf/bin/ld: cannot find -locl_util
/home/user/Vijay_HS/UACE_2030/sdk-linux/linux-devkit/sysroots/x86_64-arago-linux/usr/bin/../lib/gcc/arm-linux-gnueabihf/8.3.0/../../../../arm-linux-gnueabihf/bin/ld: cannot find -lm
collect2: error: ld returned 1 exit status
Makefile:7: recipe for target 'simple' failed
make[1]: *** [simple] Error 1
I think, OpenCL is not installed in my Ubuntu machine, and thats the reason these errors are occuring. I tried to install ti-opencl, but it is failing, looks like this is obsolete. Can I please get some help in installing the OpenCL components and resolving these errors. I am stuck with my project here, kindly please help me on priority.
Thanks & Regards
Vijay H.S