Part Number: AM6546
Tool/software: WEBENCH® Design Tools
Hi TI team,
I have used latest given BSDL file for boundary scan testing.
Yet issue about DDR4 is not yet solved. Can you please Look in to this DDR4 section of the BSDL.
It showing DQS signals never toggle, which has to change its state.
Please do look into this on Priority basis.
Also we are are not able to test Ethernet IC which is connected using MCU_RGMII.
Do we need additional BSDL file for boundary scan this Ethernet section.
We are testing AM6546 EVM board using boundary scan.
Here, We are able to test U31 and U88, which are connected using PRG2_RGMII_x interface.
But, we are not able to read PHY chip ID of U22 which is connected using MCU_RGMII interface.
|
Part Number |
DP83867IRRGZ |
DP83867IRRGZ |
DP83867IRRGZ |
|
Chip Reference Number |
U22 |
U88 |
U31 |
|
Interface |
RGMII_ETHERNET_PHY_MCU |
PRG2_RGMII_2 |
PRG2_RGMII_1 |
|
PHY chip id |
Not able to read ( Getting value as 0xFF) |
Able to Read |
Able to Read |
|
RX clock detection |
Not able to detect |
Able to Detect |
Able to Detect |
|
Link Up/LinkDown activity |
Not able to detect |
Able to Detect |
Able to Detect |
Regards,
Jagrutee