Other Parts Discussed in Thread: OMAPL138, FLASHTOOL
With the OMAP-L138, we have encountered issues with the onchip boot loader (RBL) when incorporating various different flash devices that should be compatible.
However, if we had more detailed information, or maybe even the OMAP-L138 RBL source code, we could easily figure out the required specifications for supported boot up flash devices. Any chance we can obtain the OMAP-L138 RBL source code or something to help us find out more details as to the supported flash device specifications?
Interestingly, the RBL code for the Keystone C667x was also initially closed, but eventually released therefore making it easy to understand boot device compatibility.
Hope to hear from you soon.
Regards,
Robert