Hello, everyone,
My DM6467T dvevm use linux-davinci-staging 2.6.32-rc2.
When I receive UDP packets in Gbit mode, there are many packets are lost.
So I download a new arogo kernel linux-davinci-staging 2.6.32.17, but it need related file system, such as "arago-demo-image-dm6467t-evm.tar.gz".
Where can I download this file system?
Or, Is there a simple method to resolve the UDP packets loss problem in Gbit mode?
Thanks to you!