Other Parts Discussed in Thread: AM5748
Hello!
I use ti-processor-sdk-linux-am57xx-evm-06.03.00.106 on am5749(custom board).
Everything is work fine but I would like to know what is the reason for this warnings.How to resolve it?
Boot log:
U-Boot 2019.01-g54a57c4-dirty (Aug 24 2020 - 09:44:31 +0200)
CPU : DRA762-GP ES1.0 ABZ package
Model: TI AM5748 IDK
Board: AM574x IDK REV 1.0A
DRAM: 2 GiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
Loading Environment from FAT... *** Warning - bad CRC, using default environment
Loading Environment from MMC... Card did not respond to voltage select!
*** Warning - No block device, using default environment
Card did not respond to voltage select!
invalid mmc device
am57x_idk_lcd_detect: Failed to get I2C device 0/56 (ret 1)
Net:
Warning: ethernet@48484000 using MAC address from ROM
eth0: ethernet@48484000
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
** Unable to read file boot.scr **
1490 bytes read in 2 ms (727.5 KiB/s)
Loaded env from uEnv.txt
Importing environment from mmc0 ...
Running uenvcmd ...
1 bytes read in 1 ms (1000 Bytes/s)
Already setup.
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
4452864 bytes read in 199 ms (21.3 MiB/s)
89486 bytes read in 6 ms (14.2 MiB/s)
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 8ffe7000, end 8ffffd8d ... OK
Starting kernel ...
BR,
Oleg