This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6548: Connections for Unused Pins

Part Number: AM6548

For pins not mentioned in "4.5 Connections for Unused Pins" on the data sheet, how is it recommended to connect each of the pins when unused?

Most of pins with a Pad Configuration Register can be left unconnected with their multiplexing mode set to GPIO input and internal pulldown resistor enabled.

For pins without a Pad Configuration Register, which are MUXMODE is blank and TYPE have Input or Analog in "Table 4-1. Pin Attributes" on the data sheet, is an external pull resistor required to hold a valid logic level?

BALL NUMBER BALL NAME
G28 CSI0_RXN0
H27 CSI0_RXN1
F26 CSI0_RXN2
H25 CSI0_RXN3
G24 CSI0_RXN4
F28 CSI0_RXP0
G27 CSI0_RXP1
G26 CSI0_RXP2
G25 CSI0_RXP3
F24 CSI0_RXP4
A10 DDR_AC0
D9 DDR_AC1
C9 DDR_AC2
E9 DDR_AC3
A9 DDR_AC4
E8 DDR_AC5
F8 DDR_AC6
C7 DDR_AC7
C8 DDR_AC8
D7 DDR_AC9
E7 DDR_AC10
A6 DDR_AC11
F7 DDR_AC12
D6 DDR_AC13
C6 DDR_AC14
F6 DDR_AC15
E6 DDR_AC16
E5 DDR_AC17
D8 DDR_AC18
D10 DDR_AC19
E10 DDR_AC20
C10 DDR_AC21
F11 DDR_AC22
B10 DDR_AC23
D11 DDR_AC24
B11 DDR_AC25
C11 DDR_AC26
E11 DDR_AC27
E12 DDR_AC28
D12 DDR_AC29
D5 DDR_ALERTn
B8 DDR_CK0N
A8 DDR_CK0P
B7 DDR_CK1N
A7 DDR_CK1P
E1 DDR_DM0
C5 DDR_DM1
D14 DDR_DM2
B17 DDR_DM3
A3 DDR_DQ0
B2 DDR_DQ1
C2 DDR_DQ2
D2 DDR_DQ3
E2 DDR_DQ4
G1 DDR_DQ5
F2 DDR_DQ6
F1 DDR_DQ7
E3 DDR_DQ8
C3 DDR_DQ9
D3 DDR_DQ10
B3 DDR_DQ11
D4 DDR_DQ12
C4 DDR_DQ13
B4 DDR_DQ14
B5 DDR_DQ15
E13 DDR_DQ16
C14 DDR_DQ17
B14 DDR_DQ18
A14 DDR_DQ19
E14 DDR_DQ20
B13 DDR_DQ21
C13 DDR_DQ22
D13 DDR_DQ23
D15 DDR_DQ24
C15 DDR_DQ25
E16 DDR_DQ26
E15 DDR_DQ27
D16 DDR_DQ28
B16 DDR_DQ29
C16 DDR_DQ30
A17 DDR_DQ31
C1 DDR_DQS0N
D1 DDR_DQS0P
A4 DDR_DQS1N
A5 DDR_DQS1P
A12 DDR_DQS2N
A13 DDR_DQS2P
A16 DDR_DQS3N
A15 DDR_DQS3P
B19 DDR_ECC_D0
B18 DDR_ECC_D1
C18 DDR_ECC_D2
D18 DDR_ECC_D3
E18 DDR_ECC_D4
E17 DDR_ECC_D5
D17 DDR_ECC_D6
C17 DDR_ECC_DM
A18 DDR_ECC_DQSN
A19 DDR_ECC_DQSP
A11 DDR_RESETn
F12 DDR_VREF0
F15 DDR_VREF_ZQ
V5 MCU_BYP_POR
L25 OLDI0_CLKN
K25 OLDI0_CLKP
J28 OLDI0_A0N
K28 OLDI0_A0P
L27 OLDI0_A1N
K27 OLDI0_A1P
K24 OLDI0_A2N
J24 OLDI0_A2P
J26 OLDI0_A3N
K26 OLDI0_A3P
E22 OSC1_XO
AF9 REFCLK0N
AF10 REFCLK0P
AE8 REFCLK1N
AE9 REFCLK1P
AE2 USB0_DM
AF1 USB0_DP
AF7 USB0_ID
AE7 USB0_VBUS
AD2 USB1_DM
AE1 USB1_DP
AF5 USB1_ID
AF6 USB1_VBUS
AC4 WKUP_LFOSC0_XO
AE6 WKUP_OSC0_XO

Best regards,

Daisuke

  • Any unused DDR strobe signals (DQS) should be terminated with external resistors.  DQS should be pulled down via 1K-ohm resistor, DQSn should be pulled up via 1K-ohm resistor.  No other DDR signals require termination.

    MCU_BYP_POR should be pulled high or low - depending on desired configuration.  It should not be left floating.

    All other signals listed should not require any external termination if unused.

  • Hi Robert-san,

    Thank you for your reply.

    Robert Eschler said:

    All other signals listed should not require any external termination if unused.

    Does what you said mean that each of the signal pins can be left unconnected (only connected to a PCB solder pad) by an internal pull resistor enabled by default?

    Best regards,

    Daisuke

  • Correct - the signals can be left unconnected (only connected to a PCB solder pad).

  • Hi Robert-san,

    Thank you for your reply.

    Robert Eschler said:

    Any unused DDR strobe signals (DQS) should be terminated with external resistors.  DQS should be pulled down via 1K-ohm resistor, DQSn should be pulled up via 1K-ohm resistor.  No other DDR signals require termination.

    Is it really correct to pull down DQS (positive) and pull up DQSn (negative)?

    In the case of AM335x they are connected in reverse.

    https://e2e.ti.com/support/processors/f/791/p/894544/3307306#3307306

    "When not using all or part of a DDR3 interface, the proper method of handling the unused pins is to tie off the DDR_DQS[x] pins to the VDDS_DDR supply via a 1-kΩ resistor and pulling the DDR_DQSn[x] pins to ground via a 1k-Ω resistor."

    Best regards,

    Daisuke

  • Which signals is pulled up or down is not critical, as long as they are pulled in opposite directions.

  • Hi Robert-san,

    Thank you for your reply.

    I understand they are pulled in opposite directions that is, pull down DQS (positive) and pull up DQSn (negative).

    I was confused because it was suggested that they are pulled in identical directions in the case of AM335x.

    Best regards,

    Daisuke