Part Number: TDA4VMXEVM
Dear Sir/Madam,
I use PSDKRA 7.0 and psdk_rtos_auto_ti_data_set_ptk_06_02_00.tar.gz.
I tried to run "Radar Group Tracker Demo" on TDA4VMXEVM.
But it can't run success.
Following are the log messages.
root@j7-evm:/opt/vision_apps# ./vx_app_radar_gtrack.out --cfg app.cfg
APP: Init ... !!!
MEM: Init ... !!!
MEM: Initialized DMA HEAP (fd=4) !!!
MEM: Init ... Done !!!
IPC: Init ... !!!
IPC: Init ... Done !!!
REMOTE_SERVICE: Init ... !!!
REMOTE_SERVICE: Init ... Done !!!
APP: Init ... Done !!!
3330.475978 s: VX_ZONE_INIT:Enabled
3330.475994 s: VX_ZONE_ERROR:Enabled
3330.476000 s: VX_ZONE_WARNING:Enabled
3330.476534 s: VX_ZONE_INIT:[tivxInit:71] Initialization Done !!!
3330.476751 s: VX_ZONE_INIT:[tivxHostInit:48] Initialization Done for HOST !!
ERROR in sensorstream: Cannot open file /opt/vision_apps/test_data_ptk/sequencet
Assertion `0` failed on line 96 in /home/gtbldadm/nightlybuilds/psdk_rtos_auto/p
root@j7-evm:/opt/vision_apps#
Could you give me suggestion to fix the error?
Best regards
-Jason