This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6727 UHPI read timing

Hi,

I have a question about UHPI read timing.

Figure 4-23 of SPRS370C Multiplexed read timing with /UHPI_HAS held high is described.

When HPID read with auto-increment and read FIFO initially empty

I understood that No.1 - Case 3 of Table4-18 is used as delay time when 1st half word is read.

But when 2nd half word is read which case of No.1 is used as delay time?

I think when 1st half word is read, FIFO is filled with data.

So I think case 4 would be used. Is this correct?

 

Best regards,

Tak