This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: TDA4VM : Weston is killed and launched during linux boot.

Part Number: TDA4VM

Hi TI Support. 

We are using ti-processor-sdk-linux-automotive-j7-evm-07_00_01 on J7ES, The Linux Yocto image was built using bitbake tisdk-default-image. 

We observed that the weston is launched twice.

1) using weston-launch command from systemd service (using weston.ini file etc/xdg/weston/weston.ini ) 

2) using etc/init.d/weston script after the Linux boots to login prompt (using weston.ini file etc/weston.ini)

we observed below issues. 

1) The weston desktop is displayed during boot (with grey wallpaper), but after the boot is done we can see only the agetty console on display.

2) Sometimes the weston launched by weston-launch is killed and then weston launched by etc/init.d/weston is running .(with the ti board wallpaper)

3) Sometimes the weston launched by weston-launch is not killed. and we are seeing only agetty console on the display. 

This issue was not observed in 06_00_02 version.

Best Regards

Sami