Hi All,
Is there Any Davinci EVM which has HDMI interface?
I want to integrate Si9022 HDMI as the ONscreenDisplay for DM368, is it possible?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Ashwani,
Based on past responses from similar questions, HDMI connectivity with the DM368 should work, although there doesn't exist such a reference designed. If the Si9022 supports the same physical interface (i.e. ITU.656) to connect to the DM368, which appears it does base on the datasheet, then this can be supported.
This thread has additional background information
http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/100/p/43803/153097.aspx#153097
Marcus
PS: Please mark this post as verified, if you think it has answered your question. Thanks.