DM368 datasheet only list SD/MMC card. Can DM368 support Memory stick card ?
Or we need a memory stick card controller IC for Memory Stick Card ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
DM368 datasheet only list SD/MMC card. Can DM368 support Memory stick card ?
Or we need a memory stick card controller IC for Memory Stick Card ?
If by memory stick you are referring to USB Mass Storage Devices then yes, the DM368 USB IP supports it.
I mean sony memory stick card.
Can DM368 connect to memory stick card interface directly like SD card ?
Or need a memory stick card controller ?
Thanks
I have the same question. From the description of OMAP3430 Software Development Platform, it seems that OMAP 3430 supports Memory Stick through its 1.8V/3V Media Card I/F. Can you confirm that such feature does not exists on DM368? If Memory Stick cannot be supported by DM368 natively, is there a TI card reader chip that can be used to support both Memory Stick varieties and MMC/SD with TI recommended Linux driver?