Part Number: AM3359
Hi All,
I am unable to boot successfully to the Linux kernel from the in built NAND Flash on our custom board based on the ICE_V2 board. Nand flash used is MT29F4G08ABADAWP-IT.
I am getting the below msg in the bootLog
[FAILED] Failed to start Load Kernel Modules.
Attaching full boot log :
U-Boot SPL 2018.01 (Sep 01 2020 - 11:21:14)
Trying to boot from NAND
U-Boot 2018.01 (Sep 01 2020 - 11:21:14 +0530)
CPU : AM335X-GP rev 2.1
Model: TI AM3359 ICE-V2
DRAM: 512 MiB
NAND: 512 MiB
MMC:
Net: Could not get PHY for cpsw: addr 0
cpsw, usb_ether
Hit any key to stop autoboot: 0
Booting from nand ...
NAND read: device 0 offset 0x80000, size 0x40000
262144 bytes read: OK
NAND read: device 0 offset 0x200000, size 0x800000
8388608 bytes read: OK
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 8fff3000, end 8ffff905 ... OK
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 4.14.67-gd315a9bb00 (astra@astra-B250M-D3H) (gcc version 7.2.1 20171011 (Linaro GCC 7.2-2017.11)) #97 P9
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] OF: fdt: Machine model: TI AM3359 ICE-V2
[ 0.000000] Memory policy: Data cache writeback
[ 0.000000] efi: Getting EFI parameters from FDT:
[ 0.000000] efi: UEFI not found.
[ 0.000000] cma: Reserved 48 MiB at 0x9d000000
[ 0.000000] CPU: All CPU(s) started in SVC mode.
[ 0.000000] AM335X ES2.1 (sgx neon)
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 129920
[ 0.000000] Kernel command line: console=ttyO0,115200n8 root=ubi0:rootfs rw ubi.mtd=NAND.file-system,2048 rootfstype=ubifs rootwa1
[ 0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Memory: 456912K/524288K available (8192K kernel code, 318K rwdata, 2480K rodata, 1024K init, 275K bss, 18224K reserve)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
[ 0.000000] vmalloc : 0xe0800000 - 0xff800000 ( 496 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xe0000000 ( 512 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0xc0008000 - 0xc0900000 (9184 kB)
[ 0.000000] .init : 0xc0c00000 - 0xc0d00000 (1024 kB)
[ 0.000000] .data : 0xc0d00000 - 0xc0d4fbd8 ( 319 kB)
[ 0.000000] .bss : 0xc0d4fbd8 - 0xc0d94964 ( 276 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] Tasks RCU enabled.
[ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[ 0.000000] OMAP clockevent source: timer2 at 25000000 Hz
[ 0.000017] sched_clock: 32 bits at 25MHz, resolution 40ns, wraps every 85899345900ns
[ 0.000037] clocksource: timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 76450417870 ns
[ 0.000049] OMAP clocksource: timer1 at 25000000 Hz
[ 0.000238] timer_probe: no matching timers found
[ 0.000458] Console: colour dummy device 80x30
[ 0.000489] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
[ 0.000497] This ensures that you still see kernel messages. Please
[ 0.000503] update your kernel commandline.
[ 0.000536] Calibrating delay loop... 795.44 BogoMIPS (lpj=3977216)
[ 0.089067] pid_max: default: 32768 minimum: 301
[ 0.089266] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.089282] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.090103] CPU: Testing write buffer coherency: ok
[ 0.090885] Setting up static identity map for 0x80100000 - 0x80100060
[ 0.091056] Hierarchical SRCU implementation.
[ 0.091423] EFI services will not be available.
[ 0.092869] devtmpfs: initialized
[ 0.101716] random: get_random_u32 called from bucket_table_alloc+0x8c/0x1ac with crng_init=0
[ 0.102233] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 0.102546] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.102571] futex hash table entries: 256 (order: -1, 3072 bytes)
[ 0.106555] pinctrl core: initialized pinctrl subsystem
[ 0.107358] DMI not present or invalid.
[ 0.107783] NET: Registered protocol family 16
[ 0.110240] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.124992] omap_hwmod: debugss: _wait_target_disable failed
[ 0.177589] cpuidle: using governor ladder
[ 0.177632] cpuidle: using governor menu
[ 0.181896] GPIO line 7 (FET_SWITCH_CTRL) hogged as output/high
[ 0.182341] OMAP GPIO hardware version 0.1
[ 0.191004] omap-gpmc 50000000.gpmc: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/nandflash_pins_se
[ 0.193101] No ATAGs?
[ 0.193117] hw-breakpoint: debug architecture 0x4 unsupported.
[ 0.206666] edma 49000000.edma: TI EDMA DMA engine driver
[ 0.210590] omap_i2c 44e0b000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/i2c0_pins_default,e
[ 0.210661] omap_i2c 4802a000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/i2c1_pins_default,e
[ 0.210785] media: Linux media interface: v0.10
[ 0.210835] Linux video capture interface: v2.00
[ 0.210947] pps_core: LinuxPPS API ver. 1 registered
[ 0.210956] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.210979] PTP clock support registered
[ 0.211014] EDAC MC: Ver: 3.0.0
[ 0.211501] dmi: Firmware registration failed.
[ 0.211934] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400
[ 0.212305] Advanced Linux Sound Architecture Driver Initialized.
[ 0.213549] clocksource: Switched to clocksource timer1
[ 0.222316] NET: Registered protocol family 2
[ 0.223098] TCP established hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.223151] TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.223198] TCP: Hash tables configured (established 4096 bind 4096)
[ 0.223301] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 0.223321] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 0.223517] NET: Registered protocol family 1
[ 0.224068] RPC: Registered named UNIX socket transport module.
[ 0.224084] RPC: Registered udp transport module.
[ 0.224091] RPC: Registered tcp transport module.
[ 0.224098] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.225042] hw perfevents: no interrupt-affinity property for /pmu, guessing.
[ 0.225175] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counters available
[ 0.226717] workingset: timestamp_bits=14 max_order=17 bucket_order=3
[ 0.231196] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.232034] NFS: Registering the id_resolver key type
[ 0.232087] Key type id_resolver registered
[ 0.232097] Key type id_legacy registered
[ 0.232148] ntfs: driver 2.1.32 [Flags: R/O].
[ 0.234510] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245)
[ 0.234534] io scheduler noop registered
[ 0.234543] io scheduler deadline registered
[ 0.234786] io scheduler cfq registered (default)
[ 0.234800] io scheduler mq-deadline registered
[ 0.234808] io scheduler kyber registered
[ 0.236205] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568
[ 0.289672] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled
[ 0.292908] 44e09000.serial: ttyS0 at MMIO 0x44e09000 (irq = 30, base_baud = 3000000) is a 8250
[ 0.943566] console [ttyS0] enabled
[ 0.948220] 48022000.serial: ttyS1 at MMIO 0x48022000 (irq = 31, base_baud = 3000000) is a 8250
[ 0.958083] 481aa000.serial: ttyS5 at MMIO 0x481aa000 (irq = 32, base_baud = 3000000) is a 8250
[ 0.968698] omap_rng 48310000.rng: Random Number Generator ver. 20
[ 0.987565] brd: module loaded
[ 0.997579] loop: module loaded
[ 1.004760] m25p80 spi1.0: n25q256 (32768 Kbytes)
[ 1.009525] 1 ofpart partitions found on MTD device spi1.0
[ 1.015164] Creating 1 MTD partitions on "spi1.0":
[ 1.019987] 0x000000000000-0x000002000000 : "spi1_partition"
[ 1.027694] libphy: Fixed MDIO Bus: probed
[ 1.103639] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6, bus freq 1000000
[ 1.111352] libphy: 4a101000.mdio: probed
[ 1.115900] davinci_mdio: probe of 4a101000.mdio failed with error -5
[ 1.123177] cpsw 4a100000.ethernet: Detected MACID = 68:47:49:7d:74:b4
[ 1.129912] cpsw 4a100000.ethernet: initialized cpsw ale version 1.4
[ 1.136329] cpsw 4a100000.ethernet: ALE Table size 1024
[ 1.141615] cpsw 4a100000.ethernet: cpts: overflow check period 500 (jiffies)
[ 1.149675] cpsw 4a100000.ethernet: cpsw: Detected MACID = 68:47:49:7d:74:b6
[ 1.158394] i2c /dev entries driver
[ 1.162375] IR NEC protocol handler initialized
[ 1.167100] IR RC5(x/sz) protocol handler initialized
[ 1.172178] IR RC6 protocol handler initialized
[ 1.176748] IR JVC protocol handler initialized
[ 1.181295] IR Sony protocol handler initialized
[ 1.185944] IR SANYO protocol handler initialized
[ 1.190665] IR Sharp protocol handler initialized
[ 1.195400] IR MCE Keyboard/mouse protocol handler initialized
[ 1.201255] IR XMP protocol handler initialized
[ 1.207788] cpuidle: enable-method property 'ti,am3352' found operations
[ 1.215014] sdhci: Secure Digital Host Controller Interface driver
[ 1.221226] sdhci: Copyright(c) Pierre Ossman
[ 1.226021] sdhci-pltfm: SDHCI platform and OF driver helper
[ 1.232290] ledtrig-cpu: registered to indicate activity on CPUs
[ 1.241809] NET: Registered protocol family 10
[ 1.248015] Segment Routing with IPv6
[ 1.251786] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[ 1.258583] NET: Registered protocol family 17
[ 1.263336] Key type dns_resolver registered
[ 1.267994] omap_voltage_late_init: Voltage driver support not added
[ 1.280037] omap-gpmc 50000000.gpmc: GPMC revision 6.0
[ 1.285412] gpmc_mem_init: disabling cs 0 mapped at 0x0-0x1000000
[ 1.293184] nand: device found, Manufacturer ID: 0x2c, Chip ID: 0xdc
[ 1.299736] nand: Micron MT29F4G08ABADAWP
[ 1.303816] nand: 512 MiB, SLC, erase size: 128 KiB, page size: 2048, OOB size: 64
[ 1.311516] nand: using OMAP_ECC_BCH8_CODE_HW ECC scheme
[ 1.317017] 10 ofpart partitions found on MTD device omap2-nand.0
[ 1.323139] Creating 10 MTD partitions on "omap2-nand.0":
[ 1.328597] 0x000000000000-0x000000020000 : "NAND.SPL"
[ 1.334971] 0x000000020000-0x000000040000 : "NAND.SPL.backup1"
[ 1.341712] 0x000000040000-0x000000060000 : "NAND.SPL.backup2"
[ 1.348587] 0x000000060000-0x000000080000 : "NAND.SPL.backup3"
[ 1.355377] 0x000000080000-0x0000000c0000 : "NAND.u-boot-spl-os"
[ 1.362326] 0x0000000c0000-0x0000001c0000 : "NAND.u-boot"
[ 1.369101] 0x0000001c0000-0x0000001e0000 : "NAND.u-boot-env"
[ 1.375811] 0x0000001e0000-0x000000200000 : "NAND.u-boot-env.backup1"
[ 1.383146] 0x000000200000-0x000000a00000 : "NAND.kernel"
[ 1.393207] 0x000000a00000-0x000010000000 : "NAND.file-system"
[ 1.514702] gpmc_read_settings_dt: page/burst-length set but not used!
[ 1.553985] tps65910 0-002d: No interrupt support, no core IRQ
[ 1.563453] vrtc: supplied by vbat
[ 1.571178] vio: supplied by vbat
[ 1.576152] vdd1: supplied by vbat
[ 1.581505] vdd2: supplied by vbat
[ 1.587020] random: fast init done
[ 1.591966] vdig1: supplied by vbat
[ 1.596894] vdig2: supplied by vbat
[ 1.601754] vpll: supplied by vbat
[ 1.606650] vdac: supplied by vbat
[ 1.611489] vaux1: supplied by vbat
[ 1.616410] vaux2: supplied by vbat
[ 1.621271] vaux33: supplied by vbat
[ 1.626333] vmmc: supplied by vbat
[ 1.631170] vbb: supplied by vbat
[ 1.636397] pca953x 0-0041: 0-0041 supply vcc not found, using dummy regulator
[ 1.643876] pca953x 0-0041: failed reading register
[ 1.648984] pca953x: probe of 0-0041 failed with error -121
[ 1.654851] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz
[ 1.661909] omap_i2c 4802a000.i2c: bus 1 rev0.11 at 500 kHz
[ 1.668010] ubi0: attaching mtd10
[ 2.854211] ubi0: scanning is finished
[ 2.877302] ubi0: attached mtd10 (name "NAND.file-system", size 246 MiB)
[ 2.884349] ubi0: PEB size: 131072 bytes (128 KiB), LEB size: 126976 bytes
[ 2.891257] ubi0: min./max. I/O unit sizes: 2048/2048, sub-page size 512
[ 2.898017] ubi0: VID header offset: 2048 (aligned 2048), data offset: 4096
[ 2.905048] ubi0: good PEBs: 1968, bad PEBs: 0, corrupted PEBs: 0
[ 2.911169] ubi0: user volume: 1, internal volumes: 1, max. volumes count: 128
[ 2.918442] ubi0: max/mean erase counter: 2/0, WL threshold: 4096, image sequence number: 935963569
[ 2.927561] ubi0: available PEBs: 0, total reserved PEBs: 1968, PEBs reserved for bad PEB handling: 80
[ 2.936935] ubi0: background thread "ubi_bgt0d" started, PID 44
[ 2.943230] hctosys: unable to open rtc device (rtc0)
[ 2.949163] ALSA device list:
[ 2.952157] No soundcards found.
[ 2.963666] UBIFS (ubi0:0): background thread "ubifs_bgt0_0" started, PID 45
[ 3.042111] UBIFS (ubi0:0): recovery needed
[ 3.246750] UBIFS (ubi0:0): recovery completed
[ 3.251591] UBIFS (ubi0:0): UBIFS: mounted UBI device 0, volume 0, name "rootfs"
[ 3.259071] UBIFS (ubi0:0): LEB size: 126976 bytes (124 KiB), min./max. I/O unit sizes: 2048 bytes/2048 bytes
[ 3.269180] UBIFS (ubi0:0): FS size: 237826048 bytes (226 MiB, 1873 LEBs), journal size 9023488 bytes (8 MiB, 72 LEBs)
[ 3.279951] UBIFS (ubi0:0): reserved for root: 0 bytes (0 KiB)
[ 3.285850] UBIFS (ubi0:0): media format: w4/r0 (latest is w5/r0), UUID C8F4E3B6-7FEB-486F-ABEC-EEF47A9446C1, small LPT model
[ 3.297933] VFS: Mounted root (ubifs filesystem) on device 0:14.
[ 3.305725] devtmpfs: mounted
[ 3.310192] Freeing unused kernel memory: 1024K
[ 3.403604] NOHZ: local_softirq_pending 40
[ 3.543617] NOHZ: local_softirq_pending 40
[ 3.563583] NOHZ: local_softirq_pending 202
[ 3.648422] systemd[1]: System time before build time, advancing clock.
[ 3.673593] NOHZ: local_softirq_pending 40
[ 3.713602] NOHZ: local_softirq_pending 40
[ 3.771777] systemd[1]: systemd 234 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPT)
[ 3.794070] systemd[1]: Detected architecture arm.
Welcome to Arago 2018.08!
[ 3.836664] systemd[1]: Set hostname to <am335x-evm>.
[ 3.853613] NOHZ: local_softirq_pending 202
[ 4.303620] NOHZ: local_softirq_pending 40
[ 4.323627] NOHZ: local_softirq_pending 40
[ 4.383605] NOHZ: local_softirq_pending 40
[ 4.653652] NOHZ: local_softirq_pending 40
[ 4.693933] random: systemd: uninitialized urandom read (16 bytes read)
[ 4.703327] systemd[1]: Listening on Journal Socket.
[ OK ] Listening on Journal Socket.
[ 4.735435] random: systemd: uninitialized urandom read (16 bytes read)
[ 4.742786] systemd[1]: Listening on Journal Socket (/dev/log).
[ OK ] Listening on Journal Socket (/dev/log).
[ 4.775156] random: systemd: uninitialized urandom read (16 bytes read)
[ 4.782106] systemd[1]: Listening on Network Service Netlink Socket.
[ OK ] Listening on Network Service Netlink Socket.
[ 4.841464] systemd[1]: Listening on Process Core Dump Socket.
[ OK ] Listening on Process Core Dump Socket.
[ 4.874530] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[ OK ] Started Dispatch Password Requests to Console Directory Watch.
[ 4.926530] systemd[1]: Created slice User and Session Slice.
[ OK ] Created slice User and Session Slice.
[ 4.956064] systemd[1]: Listening on udev Kernel Socket.
[ OK ] Listening on udev Kernel Socket.
[ OK ] Listening on udev Control Socket.
[ OK ] Reached target Remote File Systems.
[ OK ] Created slice System Slice.
[ OK ] Created slice system-serial\x2dgetty.slice.
[ OK ] Reached target Slices.
[ OK ] Created slice system-getty.slice.
Mounting Kernel Debug File System...
Starting Load Kernel Modules...
Mounting POSIX Message Queue File System...
[ OK ] Listening on Syslog Socket.
[ 5.330526] cryptodev: loading out-of-tree module taints kernel.
[ 5.337337] cryptodev: disagrees about version of symbol crypto_alloc_aead
[ 5.351282] cryptodev: Unknown symbol crypto_alloc_aead (err -22)
[ 5.351325] cryptodev: disagrees about version of symbol crypto_aead_setauthsize
[ 5.351331] cryptodev: Unknown symbol crypto_aead_setauthsize (err -22)
[ 5.351420] cryptodev: disagrees about version of symbol crypto_aead_setkey
[ 5.351425] cryptodev: Unknown symbol crypto_aead_setkey (err -22)
[ 5.351623] cryptodev: disagrees about version of symbol crypto_alloc_skcipher
[ 5.351628] cryptodev: Unknown symbol crypto_alloc_skcipher (err -22)
Starting Journal Service...
[ OK ] Started Forward Password Requests to Wall Directory Watch.
Starting Remount Root and Kernel File Systems...
[ OK ] Listening on /dev/initctl Compatibility Named Pipe.
[ OK ] Reached target Paths.
[ OK ] Reached target Swap.
Mounting Temporary Directory (/tmp)...
[ OK ] Mounted Kernel Debug File System.
[ OK ] Mounted POSIX Message Queue File System.
[ OK ] Mounted Temporary Directory (/tmp).
[ OK ] Started Journal Service.
[FAILED] Failed to start Load Kernel Modules.
See 'systemctl status systemd-modules-load.service' for details.
[ OK ] Started Remount Root and Kernel File Systems.
Starting Rebuild Hardware Database...
Starting Create System Users...
Starting Apply Kernel Variables...
Mounting Kernel Configuration File System...
Starting Flush Journal to Persistent Storage...
[ OK ] Mounted Kernel Configuration File System.
[ 6.169023] sch_fq_codel: disagrees about version of symbol tcf_block_get
[ 6.176066] sch_fq_codel: Unknown symbol tcf_block_get (err -22)
[ 6.182215] sch_fq_codel: disagrees about version of symbol gnet_stats_copy_queue
[ 6.199588] sch_fq_codel: Unknown symbol gnet_stats_copy_queue (err -22)
[ OK ] Started Create System Users.
[ 6.218908] sch_fq_codel: disagrees about version of symbol rtnl_kfree_skbs
[ 6.233719] sch_fq_codel: Unknown symbol rtnl_kfree_skbs (err -22)
[ 6.240210] sch_fq_codel: disagrees about version of symbol tcf_classify
[ 6.255448] sch_fq_codel: Unknown symbol tcf_classify (err -22)
[ 6.277087] sch_fq_codel: disagrees about version of symbol kfree_skb
[ 6.277100] sch_fq_codel: Unknown symbol kfree_skb (err -22)
[ 6.277121] sch_fq_codel: disagrees about version of symbol __skb_get_hash
[ 6.277126] sch_fq_codel: Unknown symbol __skb_get_hash (err -22)
[ 6.277134] sch_fq_codel: disagrees about version of symbol unregister_qdisc
[ 6.277138] sch_fq_codel: Unknown symbol unregister_qdisc (err -22)
[ 6.277167] sch_fq_codel: disagrees about version of symbol gnet_stats_copy_app
[ 6.290797] sch_fq_codel: Unknown symbol gnet_stats_copy_app (err -22)
[ 6.290827] sch_fq_codel: disagrees about version of symbol qdisc_tree_reduce_backlog
[ 6.290833] sch_fq_codel: Unknown symbol qdisc_tree_reduce_backlog (err -22)
[ 6.290854] sch_fq_codel: disagrees about version of symbol register_qdisc
[ 6.290859] sch_fq_codel: Unknown symbol register_qdisc (err -22)
Starting Create Static Device Nodes in /dev...
[ OK ] Started Apply Kernel Variables.
[ 6.538727] systemd-journald[59]: Received request to flush runtime journal from PID 1
[ OK ] Started Create Static Device Nodes in /dev.
[ OK ] Reached target Local File Systems (Pre).
Mounting /var/volatile...
[ 6.657424] Unable to handle kernel paging request at virtual address 6e756f0a
[ 6.667370] pgd = db060000
[ 6.675052] [6e756f0a] *pgd=00000000
[ 6.678673] Internal error: Oops: 5 [#1] PREEMPT ARM
[ 6.683658] Modules linked in:
[ 6.686736] CPU: 0 PID: 74 Comm: mount Tainted: G O 4.14.67-gd315a9bb00 #97
[ 6.694859] Hardware name: Generic AM33XX (Flattened Device Tree)
[ 6.700978] task: dc7ce400 task.stack: db05a000
[ 6.705550] PC is at kmem_cache_alloc+0x144/0x184
[ 6.710278] LR is at sget_userns+0x144/0x4a0
[ 6.714565] pc : [<c020fa7c>] lr : [<c0223b28>] psr: 200b0013
[ 6.720857] sp : db05bdf8 ip : db05be20 fp : db05be1c
[ 6.726101] r10: 00000000 r9 : 00000020 r8 : 0000017d
[ 6.731347] r7 : ffffe000 r6 : 014280c0 r5 : db00f800 r4 : dc001a80
[ 6.737902] r3 : 00000000 r2 : 0000017c r1 : a00b0013 r0 : 6e756f0a
[ 6.744458] Flags: nzCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment none
[ 6.751623] Control: 10c5387d Table: 9b060019 DAC: 00000051
[ 6.757393] Process mount (pid: 74, stack limit = 0xdb05a208)
[ 6.763163] Stack: (0xdb05bdf8 to 0xdb05c000)
[ 6.767538] bde0: 00000000 c0d18910
[ 6.775754] be00: ffffe000 c0d18910 c0d0e74c 00000020 db05be64 db05be20 c0223b28 c020f944
[ 6.783970] be20: db05be44 c0222cfc 3b9aca00 014280c0 c0d78cd0 00000000 db05be54 00000000
[ 6.792186] be40: c0d18910 00000000 c0222cfc c0d18910 00000020 00000001 db05be8c db05be68
[ 6.800402] be60: c0223eec c02239f0 c0d0e74c 00000000 c01ddf5c 00000000 c01de1f0 dc6ee000
[ 6.808619] be80: db05beb4 db05be90 c0223f34 c0223e90 00000000 c0d1a864 c01ddf5c dc776d80
[ 6.816835] bea0: 00000000 c0d18910 db05bec4 db05beb8 c01ddf78 c0223f0c db05bef4 db05bec8
[ 6.825052] bec0: c0224c30 c01ddf68 dc776dc0 c0d18910 dc776d80 db025400 dc776d80 00000000
[ 6.833268] bee0: c0d18910 dc6ee000 db05bf1c db05bef8 c0244714 c0224c20 c0d18910 dc6ee000
[ 6.841484] bf00: 00000020 dc776d80 dc776dc0 00000020 db05bf74 db05bf20 c0247474 c02446d0
[ 6.849699] bf20: 00000000 ffffe000 c0ed0000 00000000 dc650210 db8d6cc0 00000051 db05bf58
[ 6.857916] bf40: 00000000 c0246e34 200b0013 dc776d80 dc776dc0 dc6ee000 00027178 c0ed0000
[ 6.866132] bf60: db05a000 00000000 db05bfa4 db05bf78 c0247f28 c0246edc dc6ee000 00000006
[ 6.874349] bf80: db05bfac 00027140 00000000 00027168 00000015 c0107f04 00000000 db05bfa8
[ 6.882566] bfa0: c0107d20 c0247ed8 00027140 00000000 00027168 00027178 00027130 c0ed0000
[ 6.890782] bfc0: 00027140 00000000 00027168 00000015 00000000 00000000 ffffffff b6faa770
[ 6.898997] bfe0: b6e896e1 bedfdba8 b6f78a50 b6e896ea 800b0030 00027168 00000000 00000000
[ 6.907204] Backtrace:
[ 6.909671] [<c020f938>] (kmem_cache_alloc) from [<c0223b28>] (sget_userns+0x144/0x4a0)
[ 6.917714] r9:00000020 r8:c0d0e74c r7:c0d18910 r6:ffffe000 r5:c0d18910 r4:00000000
[ 6.925496] [<c02239e4>] (sget_userns) from [<c0223eec>] (sget+0x68/0x7c)
[ 6.932315] r10:00000001 r9:00000020 r8:c0d18910 r7:c0222cfc r6:00000000 r5:c0d18910
[ 6.940177] r4:00000000
[ 6.942722] [<c0223e84>] (sget) from [<c0223f34>] (mount_nodev+0x34/0x98)
[ 6.949540] r7:dc6ee000 r6:c01de1f0 r5:00000000 r4:c01ddf5c
[ 6.955238] [<c0223f00>] (mount_nodev) from [<c01ddf78>] (shmem_mount+0x1c/0x20)
[ 6.962666] r7:c0d18910 r6:00000000 r5:dc776d80 r4:c01ddf5c
[ 6.968352] [<c01ddf5c>] (shmem_mount) from [<c0224c30>] (mount_fs+0x1c/0xac)
[ 6.975530] [<c0224c14>] (mount_fs) from [<c0244714>] (vfs_kern_mount.part.3+0x50/0x10c)
[ 6.983656] r8:dc6ee000 r7:c0d18910 r6:00000000 r5:dc776d80 r4:db025400
[ 6.990393] [<c02446c4>] (vfs_kern_mount.part.3) from [<c0247474>] (do_mount+0x5a4/0xd0c)
[ 6.998607] r9:00000020 r8:dc776dc0 r7:dc776d80 r6:00000020 r5:dc6ee000 r4:c0d18910
[ 7.006387] [<c0246ed0>] (do_mount) from [<c0247f28>] (SyS_mount+0x5c/0xc8)
[ 7.013383] r10:00000000 r9:db05a000 r8:c0ed0000 r7:00027178 r6:dc6ee000 r5:dc776dc0
[ 7.021243] r4:dc776d80
[ 7.023798] [<c0247ecc>] (SyS_mount) from [<c0107d20>] (ret_fast_syscall+0x0/0x54)
[ 7.031403] r8:c0107f04 r7:00000015 r6:00027168 r5:00000000 r4:00027140
[ 7.038137] Code: e121f001 e3500000 0a000002 e5943014 (e7903003)
[ 7.073104] Unable to handle kernel NULL pointer dereference at virtual address 00000064
[ 7.087044] UBIFS assert failed in ubifs_read_node at 988 (pid 66)
[ 7.087062] CPU: 0 PID: 66 Comm: systemd-hwdb Tainted: G D O 4.14.67-gd315a9bb00 #97
[ 7.087066] Hardware name: Generic AM33XX (Flattened Device Tree)
[ 7.087071] Backtrace:
[ 7.087115] [<c010ba48>] (dump_backtrace) from [<c010bd2c>] (show_stack+0x18/0x1c)
[ 7.087124] r7:00000000 r6:db073f00 r5:00000000 r4:dc02f000
[ 7.087139] [<c010bd14>] (show_stack) from [<c0835f08>] (dump_stack+0x24/0x28)
[ 7.087158] [<c0835ee4>] (dump_stack) from [<c036444c>] (ubifs_read_node+0x140/0x294)
[ 7.087176] [<c036430c>] (ubifs_read_node) from [<c0380cd4>] (ubifs_load_znode+0x90/0x428)
[ 7.087185] r10:00000001 r9:00000000 r8:00000000 r7:db073f90 r6:db073f00 r5:00000000
[ 7.087188] r4:dc02f000
[ 7.087200] [<c0380c44>] (ubifs_load_znode) from [<c03676e4>] (ubifs_lookup_level0+0xc0/0x1e4)
[ 7.087209] r10:00000001 r9:dc7a5d6c r8:00000000 r7:5bb815a3 r6:dc7a5dd0 r5:dc02f000
[ 7.087213] r4:dc7a5d68
[ 7.087223] [<c0367624>] (ubifs_lookup_level0) from [<c0367850>] (ubifs_tnc_locate+0x48/0x1c0)
[ 7.087232] r10:00000000 r9:db018000 r8:00000000 r7:dc02f0a8 r6:dc7a5dd0 r5:00000000
[ 7.087236] r4:dc02f000
[ 7.087245] [<c0367808>] (ubifs_tnc_locate) from [<c035967c>] (do_readpage+0x170/0x45c)
[ 7.087255] r10:db018000 r9:000019f9 r8:0000005d r7:db943588 r6:00180506 r5:00000181
[ 7.087258] r4:dcd9776c
[ 7.087266] [<c035950c>] (do_readpage) from [<c035ab10>] (ubifs_readpage+0x40/0x50c)
[ 7.087275] r10:0000005d r9:db943588 r8:0000005c r7:0000005d r6:dcd9776c r5:dc02f000
[ 7.087278] r4:dcd9776c
[ 7.087299] [<c035aad0>] (ubifs_readpage) from [<c01c5044>] (generic_file_read_iter+0x558/0xa08)
[ 7.087308] r10:0000005d r9:00000001 r8:dc7fd480 r7:dc7a5ef0 r6:dcd9776c r5:db943664
[ 7.087311] r4:dc7a5f08
[ 7.087322] [<c01c4aec>] (generic_file_read_iter) from [<c0220fd0>] (__vfs_read+0xd8/0x124)
[ 7.087332] r10:00000000 r9:00001000 r8:00000000 r7:dc7a5f78 r6:dc7a5f78 r5:dc7fd480
[ 7.087335] r4:00000000
[ 7.087342] [<c0220ef8>] (__vfs_read) from [<c02210ac>] (vfs_read+0x90/0x114)
[ 7.087349] r7:dc7a5f78 r6:004b8280 r5:dc7fd480 r4:00001000
[ 7.087357] [<c022101c>] (vfs_read) from [<c022155c>] (SyS_read+0x44/0x98)
[ 7.087365] r8:004b8280 r7:00000000 r6:0005d000 r5:dc7fd480 r4:dc7fd480
[ 7.087374] [<c0221518>] (SyS_read) from [<c0107d20>] (ret_fast_syscall+0x0/0x54)
[ 7.087384] r9:dc7a4000 r8:c0107f04 r7:00000003 r6:000005e8 r5:b6e87f41 r4:004b8118
[ 7.087400] UBIFS error (ubi0:0 pid 66): ubifs_read_node: bad node type (0 but expected 9)
[ 7.087411] UBIFS error (ubi0:0 pid 66): ubifs_read_node: bad node at LEB 0:0, LEB mapping status 1
[ 7.087415] Not a node, first 24 bytes:
[ 7.087429] 00000000: 00 4c 02 db 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 .L.........
[ 7.087435] CPU: 0 PID: 66 Comm: systemd-hwdb Tainted: G D O 4.14.67-gd315a9bb00 #97
[ 7.087439] Hardware name: Generic AM33XX (Flattened Device Tree)
[ 7.087440] Backtrace:
[ 7.087454] [<c010ba48>] (dump_backtrace) from [<c010bd2c>] (show_stack+0x18/0x1c)
[ 7.087461] r7:00000000 r6:ffffffea r5:00000000 r4:dc02f000
[ 7.087471] [<c010bd14>] (show_stack) from [<c0835f08>] (dump_stack+0x24/0x28)
[ 7.087480] [<c0835ee4>] (dump_stack) from [<c0364568>] (ubifs_read_node+0x25c/0x294)
[ 7.087490] [<c036430c>] (ubifs_read_node) from [<c0380cd4>] (ubifs_load_znode+0x90/0x428)
[ 7.087499] r10:00000001 r9:00000000 r8:00000000 r7:db073f90 r6:db073f00 r5:00000000
[ 7.087502] r4:dc02f000
[ 7.087512] [<c0380c44>] (ubifs_load_znode) from [<c03676e4>] (ubifs_lookup_level0+0xc0/0x1e4)
[ 7.087522] r10:00000001 r9:dc7a5d6c r8:00000000 r7:5bb815a3 r6:dc7a5dd0 r5:dc02f000
[ 7.087525] r4:dc7a5d68
[ 7.087535] [<c0367624>] (ubifs_lookup_level0) from [<c0367850>] (ubifs_tnc_locate+0x48/0x1c0)
[ 7.087544] r10:00000000 r9:db018000 r8:00000000 r7:dc02f0a8 r6:dc7a5dd0 r5:00000000
[ 7.087548] r4:dc02f000
[ 7.087557] [<c0367808>] (ubifs_tnc_locate) from [<c035967c>] (do_readpage+0x170/0x45c)
[ 7.087566] r10:db018000 r9:000019f9 r8:0000005d r7:db943588 r6:00180506 r5:00000181
[ 7.087569] r4:dcd9776c
[ 7.087578] [<c035950c>] (do_readpage) from [<c035ab10>] (ubifs_readpage+0x40/0x50c)
[ 7.087587] r10:0000005d r9:db943588 r8:0000005c r7:0000005d r6:dcd9776c r5:dc02f000
[ 7.087590] r4:dcd9776c
[ 7.087601] [<c035aad0>] (ubifs_readpage) from [<c01c5044>] (generic_file_read_iter+0x558/0xa08)
[ 7.087610] r10:0000005d r9:00000001 r8:dc7fd480 r7:dc7a5ef0 r6:dcd9776c r5:db943664
[ 7.087613] r4:dc7a5f08
[ 7.087623] [<c01c4aec>] (generic_file_read_iter) from [<c0220fd0>] (__vfs_read+0xd8/0x124)
[ 7.087632] r10:00000000 r9:00001000 r8:00000000 r7:dc7a5f78 r6:dc7a5f78 r5:dc7fd480
[ 7.087635] r4:00000000
[ 7.087642] [<c0220ef8>] (__vfs_read) from [<c02210ac>] (vfs_read+0x90/0x114)
[ 7.087649] r7:dc7a5f78 r6:004b8280 r5:dc7fd480 r4:00001000
[ 7.087657] [<c022101c>] (vfs_read) from [<c022155c>] (SyS_read+0x44/0x98)
[ 7.087665] r8:004b8280 r7:00000000 r6:0005d000 r5:dc7fd480 r4:dc7fd480
[ 7.087674] [<c0221518>] (SyS_read) from [<c0107d20>] (ret_fast_syscall+0x0/0x54)
[ 7.087683] r9:dc7a4000 r8:c0107f04 r7:00000003 r6:000005e8 r5:b6e87f41 r4:004b8118
[ 7.087697] UBIFS error (ubi0:0 pid 66): do_readpage: cannot read page 93 of inode 6649, error -22
[ 7.087822] Unable to handle kernel paging request at virtual address 3e30333c
[ 7.087828] pgd = db02c000
[ 7.087831] [3e30333c] *pgd=00000000
[ 7.087845] Internal error: Oops: 5 [#2] PREEMPT ARM
[ 7.087849] Modules linked in:
[ 7.087860] CPU: 0 PID: 66 Comm: systemd-hwdb Tainted: G D O 4.14.67-gd315a9bb00 #97
[ 7.087863] Hardware name: Generic AM33XX (Flattened Device Tree)
[ 7.087868] task: dc7ccc00 task.stack: dc7a4000
[ 7.087885] PC is at kmem_cache_alloc+0x144/0x184
[ 7.087890] LR is at ubifs_lookup+0x94/0x364
[ 7.087895] pc : [<c020fa7c>] lr : [<c035bc60>] psr: 200f0013
[ 7.087899] sp : dc7a5da0 ip : dc7a5dc8 fp : dc7a5dc4
[ 7.087903] r10: db94b2a8 r9 : db9213b8 r8 : 00000a8b
[ 7.087908] r7 : ffffe000 r6 : 01400040 r5 : db03fa00 r4 : dc001b40
[ 7.087913] r3 : 00000000 r2 : 00000a8a r1 : a00f0013 r0 : 3e30333c
[ 7.087920] Flags: nzCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment none
[ 7.087926] Control: 10c5387d Table: 9b02c019 DAC: 00000051
[ 7.087931] Process systemd-hwdb (pid: 66, stack limit = 0xdc7a4208)
[ 7.087936] Stack: (0xdc7a5da0 to 0xdc7a6000)
[ 7.087948] 5da0: db9433e0 dc7a5e70 db94b2a8 dc02f000 00020000 db9213b8 dc7a5e14 dc7a5dc8
[ 7.087958] 5dc0: c035bc60 c020f944 db94b2a8 c0d7cdcc 0000006c db94b2c0 db94b2d4 00000013
[ 7.087968] 5de0: 00000000 00000000 00000000 00000000 dc7a5ea8 dc7a5e70 dc7a5f5c db9433e0
[ 7.087978] 5e00: 00020000 db9213b8 dc7a5ea4 dc7a5e18 c0230048 c035bbd8 dcd9776c 014000c0
[ 7.087988] 5e20: db943588 dc7a5eb0 dc7a5e70 00000000 00000000 c0aaa0dc 00020000 ffffe000
[ 7.087998] 5e40: 00000000 00000000 00000041 db024b40 00000000 00000004 db943664 00000000
[ 7.088008] 5e60: dc7a5edc dc7a5e70 c01c52e0 c02404b0 dc7a5e70 dc7a5e70 db96d1a0 00000003
[ 7.088018] 5e80: dc7a5ea8 dc7a5f5c 00000001 c0107f04 dc7a4000 00000000 dc7a5f4c dc7a5ea8
[ 7.088028] 5ea0: c02314a0 c022f4b4 dc650210 db9213b8 8c907314 00000013 dc6ec021 dc7a5f78
[ 7.088038] 5ec0: dc650210 db8d3908 db9433e0 00000101 00000002 00000094 00000000 00000000
[ 7.088048] 5ee0: 00000000 dc7a5ee8 c0d032e4 00000003 dc034180 dc776c40 00000000 00000400
[ 7.088058] 5f00: dc7a5f3c dc7a5f10 c0241eb0 c02414cc 000a0000 000a0000 dc6ec000 00000000
[ 7.088068] 5f20: fffff000 00000002 ffffff9c 00000000 00000003 ffffff9c dc6ec000 fffff000
[ 7.088078] 5f40: dc7a5f94 dc7a5f50 c021e98c c0231440 c02223d0 c022216c dc7a5f8c 00020000
[ 7.088088] 5f60: c0140000 00000004 00000100 00000001 004b8118 00000000 00000008 00000005
[ 7.088098] 5f80: c0107f04 dc7a4000 dc7a5fa4 dc7a5f98 c021ea2c c021e830 00000000 dc7a5fa8
[ 7.088108] 5fa0: c0107d20 c021ea18 004b8118 00000000 004c0290 000a0000 000001b6 000001b6
[ 7.088118] 5fc0: 004b8118 00000000 00000008 00000005 00000000 004b80d0 004b2d6c 004b337c
[ 7.088128] 5fe0: 00000000 bea8c1cc b6e88281 b6ec3188 400f0030 004c0290 00000000 00000000
[ 7.088130] Backtrace:
[ 7.088143] [<c020f938>] (kmem_cache_alloc) from [<c035bc60>] (ubifs_lookup+0x94/0x364)
[ 7.088153] r9:db9213b8 r8:00020000 r7:dc02f000 r6:db94b2a8 r5:dc7a5e70 r4:db9433e0
[ 7.088165] [<c035bbcc>] (ubifs_lookup) from [<c0230048>] (path_openat+0xba0/0x1124)
[ 7.088174] r9:db9213b8 r8:00020000 r7:db9433e0 r6:dc7a5f5c r5:dc7a5e70 r4:dc7a5ea8
[ 7.088183] [<c022f4a8>] (path_openat) from [<c02314a0>] (do_filp_open+0x6c/0xd0)
[ 7.088193] r10:00000000 r9:dc7a4000 r8:c0107f04 r7:00000001 r6:dc7a5f5c r5:dc7a5ea8
[ 7.088196] r4:00000003
[ 7.088216] [<c0231434>] (do_filp_open) from [<c021e98c>] (do_sys_open+0x168/0x1e8)
[ 7.088223] r7:fffff000 r6:dc6ec000 r5:ffffff9c r4:00000003
[ 7.088234] [<c021e824>] (do_sys_open) from [<c021ea2c>] (SyS_open+0x20/0x24)
[ 7.088243] r9:dc7a4000 r8:c0107f04 r7:00000005 r6:00000008 r5:00000000 r4:004b8118
[ 7.088253] [<c021ea0c>] (SyS_open) from [<c0107d20>] (ret_fast_syscall+0x0/0x54)
[ 7.088264] Code: e121f001 e3500000 0a000002 e5943014 (e7903003)
[ 7.088274] ---[ end trace 0259f738d05d6025 ]---
[ 7.441686] ---[ end trace 0259f738d05d6026 ]---
[ 7.941515] pgd = dc77c000
[ 7.953709] [00000064] *pgd=00000000
[ 7.957327] Internal error: Oops: 5 [#3] PREEMPT ARM
[ 7.962311] Modules linked in:
[ 7.965389] CPU: 0 PID: 1 Comm: systemd Tainted: G D O 4.14.67-gd315a9bb00 #97
[ 7.973599] Hardware name: Generic AM33XX (Flattened Device Tree)
[ 7.979717] task: dc050000 task.stack: dc04e000
[ 7.984279] PC is at devcgroup_access_write+0x50/0x50c
[ 7.989439] LR is at 0xdb0522ff
[ 7.992591] pc : [<c03a6480>] lr : [<db0522ff>] psr: 40070013
[ 7.998882] sp : dc04fe10 ip : 00000042 fp : dc04fe64
[ 8.004126] r10: dc7ca310 r9 : 00000000 r8 : 00000000
[ 8.009372] r7 : 00000002 r6 : 00000001 r5 : 00000000 r4 : db052300
[ 8.015925] r3 : 00000042 r2 : c098fa98 r1 : db052300 r0 : 00000015
[ 8.022481] Flags: nZcv IRQs on FIQs on Mode SVC_32 ISA ARM Segment none
[ 8.029645] Control: 10c5387d Table: 9c77c019 DAC: 00000051
[ 8.035414] Process systemd (pid: 1, stack limit = 0xdc04e208)
[ 8.041271] Stack: (0xdc04fe10 to 0xdc050000)
[ 8.045648] fe00: c022f778 c022b20c dc7ca300 00000000
[ 8.053863] fe20: dc04fe44 dc04feb0 dc04fe70 00000000 00000000 c0aaa0dc 00020101 ffffe000
[ 8.062079] fe40: c0d1cc5c 00000002 db03fa00 db052300 00000000 00000000 dc04fe9c dc04fe68
[ 8.070296] fe60: c019f238 c03a643c 00000000 00000000 c020f624 c01e93a4 00000002 dc7ca300
[ 8.078512] fe80: 00000000 00000000 dc04ff78 db052300 dc04fed4 dc04fea0 c0291d48 c019f1b8
[ 8.086727] fea0: 00000000 00000000 00000019 c0291c58 db024000 dc04ff78 dc04ff78 00000000
[ 8.094943] fec0: 00000002 00000000 dc04ff44 dc04fed8 c022119c c0291c64 00000000 00000000
[ 8.103160] fee0: 00001000 00000000 00000000 00000000 5bb815a3 18701a80 5bb815a3 18701a80
[ 8.111375] ff00: 5bb815a3 18701a80 000000b8 00000000 beb4e588 b6c74bec dc04ffa4 dc04ff28
[ 8.119591] ff20: 00000002 db024000 0060ccb0 dc04ff78 00000000 00000002 dc04ff74 dc04ff48
[ 8.127808] ff40: c0221418 c0221178 000000b8 00000000 db024000 db024000 00000000 00000000
[ 8.136023] ff60: 0060ccb0 00000002 dc04ffa4 dc04ff78 c02215f4 c0221378 00000000 00000000
[ 8.144240] ff80: 00000002 0060ccb0 0060ade8 00000004 c0107f04 dc04e000 00000000 dc04ffa8
[ 8.152456] ffa0: c0107d20 c02215bc 00000002 0060ccb0 00000025 0060ccb0 00000002 00000025
[ 8.160672] ffc0: 00000002 0060ccb0 0060ade8 00000004 00000002 b6c74bec 00000025 beb4e7ac
[ 8.168888] ffe0: 00000000 beb4e5d4 b6bd9b5b b6c15538 60070030 00000025 00000000 00000000
[ 8.177096] Backtrace:
[ 8.179567] [<c03a6430>] (devcgroup_access_write) from [<c019f238>] (cgroup_file_write+0x8c/0x150)
[ 8.188569] r9:00000000 r8:00000000 r7:db052300 r6:db03fa00 r5:00000002 r4:c0d1cc5c
[ 8.196359] [<c019f1ac>] (cgroup_file_write) from [<c0291d48>] (kernfs_fop_write+0xf0/0x1d4)
[ 8.204836] r9:db052300 r8:dc04ff78 r7:00000000 r6:00000000 r5:dc7ca300 r4:00000002
[ 8.212618] [<c0291c58>] (kernfs_fop_write) from [<c022119c>] (__vfs_write+0x30/0x128)
[ 8.220573] r10:00000000 r9:00000002 r8:00000000 r7:dc04ff78 r6:dc04ff78 r5:db024000
[ 8.228434] r4:c0291c58
[ 8.230978] [<c022116c>] (__vfs_write) from [<c0221418>] (vfs_write+0xac/0x170)
[ 8.238321] r9:00000002 r8:00000000 r7:dc04ff78 r6:0060ccb0 r5:db024000 r4:00000002
[ 8.246100] [<c022136c>] (vfs_write) from [<c02215f4>] (SyS_write+0x44/0x98)
[ 8.253181] r9:00000002 r8:0060ccb0 r7:00000000 r6:00000000 r5:db024000 r4:db024000
[ 8.260968] [<c02215b0>] (SyS_write) from [<c0107d20>] (ret_fast_syscall+0x0/0x54)
[ 8.268573] r9:dc04e000 r8:c0107f04 r7:00000004 r6:0060ade8 r5:0060ccb0 r4:00000002
[ 8.276354] Code: e5936040 eb1278b4 e1a04000 e3a00015 (e5958064)
[ 8.319364] ---[ end trace 0259f738d05d6027 ]---
[ 8.364958] systemd: 21 output lines suppressed due to ratelimiting
[ 8.371436] Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b
[ 8.371436]
[ 8.380633] ---[ end Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b
[ 8.380633]
[ 52.273599] random: crng init done
[ 52.277034] random: 7 urandom warning(s) missed due to ratelimiting
[ 117.448789] systemd-journald[59]: Failed to send WATCHDOG=1 notification message: Connection refused
Thanks and Regards
Chinmay Pramod