Tool/software: TI C / C ++编译器
Hi,I builded a Yocto file system, compiled with the version of psdkla-V3.4.However, two tasks have been unpacking, and they have not been completed for about 3 days.How should I solve it?
log is here.Thanks.
# ./build-core-sdk.sh dra7xx-evm
[PSDKLA]>
[PSDKLA]> Current Directory is /home/xiaomiao.yang/psdkla_03_04_00_03/yocto-layers
[PSDKLA]> PATH is /usr/local/sbin:/usr/local/bin:/usr/sbin:/usr/bin:/sbin:/bin:/usr/games:/snap/bin:/opt/gcc-linaro-5.3-2016.02-x86_64_arm-linux-gnueabihf/bin/
[PSDKLA]> Building on hirain-PowerEdge-R740 running Linux hirain-PowerEdge-R740 4.15.0-29-generic #31-Ubuntu SMP Tue Jul 17 15:39:52 UTC 2018 x86_64 x86_64 x86_64 GNU/Linux
[PSDKLA]> Starting Yocto build at Fri Sep 4 09:55:46 CST 2020
[PSDKLA]>
[PSDKLA]> cd build
[PSDKLA]> . conf/setenv
[PSDKLA]> cp conf/local.conf conf/local.conf.pristine
[PSDKLA]> MACHINE=dra7xx-evm bitbake -k tisdk-rootfs-image
NOTE: Started PRServer with DBfile: /home/xiaomiao.yang/psdkla_03_04_00_03/yocto-layers/build/cache/prserv.sqlite3, IP: 127.0.0.1, PORT: 42837, PID: 28823
Loading cache: 100% |############################################################################################################################| ETA: 00:00:00
Loaded 2849 entries from dependency cache.
NOTE: Resolving any missing task queue dependencies
Build Configuration:
BB_VERSION = "1.30.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "Ubuntu-18.04"
TARGET_SYS = "arm-linux-gnueabi"
MACHINE = "dra7xx-evm"
DISTRO = "arago"
DISTRO_VERSION = "2016.12"
TUNE_FEATURES = "arm armv7a vfp thumb neon callconvention-hard"
TARGET_FPU = "hard"
meta-glsdk = "HEAD:66cfd8ef55344508d6e7b306259f34c05b828194"
meta-arago-distro
meta-arago-extras = "HEAD:4c01410ffde8853224567fb6078d7d9f190b942f"
meta-qt5 = "HEAD:f8584d7a7c90afc71484a40279aa3df651d0e04f"
meta-networking
meta-ruby
meta-python
meta-oe = "HEAD:55c8a76da5dc099a7bc3838495c672140cedb78e"
meta-ti = "HEAD:5f3a1169d307fec41626f850f5c700437dedbe93"
meta-linaro-toolchain
meta-optee = "HEAD:2f51d38048599d9878f149d6d15539fb97603f8f"
meta = "HEAD:bfa04fa71c47e8fe9528208848cfcec2e232777d"
NOTE: Preparing RunQueue
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
ERROR: automake-1.15-r0 do_compile: oe_runmake failed
ERROR: automake-1.15-r0 do_compile: Function failed: do_compile (log file is located at /home/xiaomiao.yang/psdkla_03_04_00_03/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/automake/1.15-r0/temp/log.do_compile.28877)
ERROR: Logfile of failure stored in: /home/xiaomiao.yang/psdkla_03_04_00_03/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/automake/1.15-r0/temp/log.do_compile.28877
Log data follows:
| DEBUG: SITE files ['endian-little', 'bit-32', 'arm-common', 'arm-32', 'common-linux', 'common-glibc', 'arm-linux', 'arm-linux-gnueabi', 'common']
| DEBUG: Executing shell function do_compile
| NOTE: make -j 16
| : && /bin/mkdir -p doc && { PATH='/home/xiaomiao.yang/psdkla_03_04_00_03/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/automake/1.15-r0/build/t/wrap:'$PATH && export PATH; } && /usr/bin/perl ../automake-1.15/doc/help2man --output=doc/automake-1.15.1 automake-1.15
| help2man: can't get `--help' info from automake-1.15
| Try `--no-discard-stderr' if option outputs to stderr
| Makefile:3687: recipe for target 'doc/automake-1.15.1' failed
| make: *** [doc/automake-1.15.1] Error 255
| WARNING: /home/xiaomiao.yang/psdkla_03_04_00_03/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/automake/1.15-r0/temp/run.do_compile.28877:1 exit 1 from 'exit 1'
| ERROR: oe_runmake failed
| ERROR: Function failed: do_compile (log file is located at /home/xiaomiao.yang/psdkla_03_04_00_03/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/automake/1.15-r0/temp/log.do_compile.28877)
ERROR: Task 6172 (/home/xiaomiao.yang/psdkla_03_04_00_03/yocto-layers/sources/oe-core/meta/recipes-devtools/automake/automake_1.15.bb, do_compile) failed with exit code '1'
Currently 2 running tasks (4157 of 7428):
0: ti-cgt-arm-native-16.9.2-r0 do_unpack (pid 28868)
1: ti-cgt-pru-native-2.1.4-r0 do_unpack (pid 28871)