This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: PROCESSOR-SDK-DRA8X-TDA4X
Hi,
When i build psdkla following ti-processor-sdk-linux-automotive-j7-evm-07_00_01/docs/linux/Overview/Top_Level_Makefile.html and do the step:
host# sudo cp board-support/u-boot_build/a72/u-boot.img board-support/u-boot_build/a72/tispl.bin board-support/u-boot_build/r5/tiboot3.bin /media/$USER/boot
I find that there has no a72 directory in board-support/u-boot_build, and only a53 and r5 directory.
So i need help, and whether i need copy a53 as a72 or some mistake i have made?
Hi Bin,
You can use the output binaries in the A53 directory directly. We will address this in the next release.
Regards
Karthik