This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PRD prolems in BIOS 5.41



Hi all,

I'm using PRD module as period 1ms and I want to change it to 0.5ms in code during rutime in the .c file, not in .tcf file.

I also have made three PRD modules such as PRD0, PRD1, PRD2, but how to call every PRD module in main or in swi?

My PRD modules also do the same thing while some parameters differs and every PRD function has set to continuous mode .

Does anyone know how?

Waiting your reply urgently!

lex

  • I am going to close this thread and mark it answered.   This is same issue as this other thread:

    http://e2e.ti.com/support/embedded/f/355/p/52751/325699.aspx#325699

     

    Seems like you have 3 threads active on the same issue.  I'm going to close the other one as well and cover all this on single thread above.    Please add content and info on the single thread above so we can track the issue better and not across 3 threads.

    Thanks,
    -Karl-