This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[OMAP-L138] Can we use MMCSD0 to connect two SD card reader slots at the same time?

Other Parts Discussed in Thread: OMAP-L138

H,

 

According to the MMCSD controller user guide for the OMAP-L138 (sprufm2b), that  the MMC controller supports one or more MMC/SD cards.

In section 2 it says, and I quote:

"In the MMC/SD mode, the MMC controller supports one or more MMC/SD cards. Regardless of the
number of cards connected, the MMC/SD controller selects one by using identification broadcast on the
data line"

Can you confirm if this feature is already supported in the OMAP-L138 Linux PSP release?