Hi Champs,
Could you please let me know the main factor for the UART spec. as follows:
1) Table 6-90. Timing Requirements for UART Receive
It shows 0.96U ns (min) and 1.05U ns (max).
I think the majority of the factor for the variation is caused by the Baud Rate with Divisor Value setting.
2) Table 6-91. Switching Characteristics Over Recommended Operating Conditions for UARTx Transmit
It shows U -2 ns (min) and U +2 ns (max).
It think this is caused by the variation for each device.
Thank you very much in advance for the factor of the tolerance.
Best regards,
Hitoshi