My customer is reaching out for thermal characterization data related to the package/pins of the TMS320C6657CZHA25.
They are asking for the following information (both package and pins)
- Specific Heat
- Density
- Thermal Conductivity
I believe the goal is to understand things such as thermal expansion, etc during soldering, and use this information to increase reliability during soldering.
There are two app notes I have found:
SPRABI3B
SPRA953C
Is it possible to infer the necessary information from these calculations, and the thermal metrics in the DS...?
Example:
Just below Table 3 from the SPRA953C App Note, there is information such as "Die Attach Impedance" and "Mold Compound Thermal Conductivity"...is this information available somewhere? (If internal, you can send me a message offline)
Otherwise, if you could provide me with the above 3 thermal metrics for package/LeadFrame(pins) I can share with the customer, that would be hugely appreciated.
Regards,
Darren