Hi,
I have .264 and .aac generated by DM368 to integrate to mp4 or mkv.
The problem is that those two files are out of sync.
It could be synchronized on the DM368 machine manually
by our engineer by playing audio referring to his own time table.
The time table contains time stamps how audio should be played,
so he can play the movie in sync.
The problem is when we combined those two files, audio and video,
to a known format such as mp4.
The result MP4 would be played in PC or any other devices than DM368 machine.
That means no programmatical help is possible.
How do I make the movie in sync?
Actually the encoded audio(aac or g711) playtime is always shorter than .264 video.
Thanks in advance for your help.