This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Need help for high signal frequency process in C6713 dsk

Dear all

                I am working on C6713 dsk. It's codec AIC23 maximum sampling rate 96Khz. For FFT , i can just use signal for process 32Khz.

But my processor clock frequency is 225MHz. Basically i want to use signal (input analog CW signal) above 10 Mhz frequency. How it is possible to do it with this kit C6713.

My EMIF port is used for external interface like LCD, control system etc.

If have any other texas DSP kit which can solve my requirement ,kindly inform me.

Your kind response will be highly appreciated.

 

Regards ..

Gopal Sarkar

Scientist