Part Number: AM4372
Tool/software: Code Composer Studio
For debugging u-boot spl, how I can I find out the offset which I need to apply when loading the symbols? No offset at all does not work for me.
This is the bdinfo output of second level u-boot:
=> bdinfo arch_number = 0x00000000 boot_params = 0x80000100 DRAM bank = 0x00000000 -> start = 0x80000000 -> size = 0x20000000 baudrate = 115200 bps TLB addr = 0x9fff0000 relocaddr = 0x9ff50000 reloc off = 0x1f750000 irq_sp = 0x9df323a0 sp start = 0x9df32390 Early malloc usage: 92c / 2000 fdt_blob = 0x9df323b8 => undefined instruction pc : [<807ffb46>] lr : [<9ff6301b>] reloc pc : [<610afb46>] lr : [<8081301b>] sp : 9df32250 ip : 9ffbcf40 fp : 00000001 r10: 0000000a r9 : 9df3feb8 r8 : 00000001 r7 : 9ffa3f39 r6 : 9ffb5528 r5 : 00000000 r4 : 9ffc2ad0 r3 : 9ff79051 r2 : 9ffbd5c4 r1 : 44e09014 r0 : 00000000 Flags: nzcv IRQs off FIQs off Mode SVC_32 Code: e1a09001 eaffffd2 ebf05a07 e0810790 (e1a09001)
I have tried to use the same relocaddr but this does not work.
Thank you and regards
Peter