Part Number: TDA2SX
Hi all,
I am working on tda2sx processor with my custom board.I am getting the below errors at MLO log.
U-Boot SPL DEBUGGING START in hwinit_common.c
Timed out in wait_for_event: status=0000
Check if pads/pull-ups of bus are properly configured
ti_i2c_eeprom_init failed 1
1150 -> optimize_vcore_voltage:efuse 0x4a003b20 bits=16 Vnom=1150, using efuse value 1070
1070
1150 -> optimize_vcore_voltage:efuse 0x4a0025f4 bits=16 Vnom=1150, using efuse value 1045
1045
0 -> 0
1250 -> optimize_vcore_voltage:efuse 0x4a003b10 bits=16 Vnom=1250, using efuse value 1075
1075
1250 -> optimize_vcore_voltage:efuse 0x4a0025e8 bits=16 Vnom=1250, using efuse value 1075
1075
1250 -> optimize_vcore_voltage:efuse 0x4a0025d4 bits=16 Vnom=1250, using efuse value 1099
1099
cor: 1045
do_scale_vcore: volt - 1045 offset_code - 0x3d
i2c_write: pads on bus probably not configured (status=0x10)
Scaling voltage failed for 0x33
IODELAY: IO delay recalibration successfully completed
mpu: 1070
do_scale_vcore: volt - 1070 offset_code - 0x3f
i2c_write: pads on bus probably not configured (status=0x10)
Scaling voltage failed for 0x23
mm: 0
gpu: 1075
do_scale_vcore: volt - 1075 offset_code - 0x40
i2c_write: pads on bus probably not configured (status=0x10)
Scaling voltage failed for 0x2f
eve: 1075
do_scale_vcore: volt - 1075 offset_code - 0x40
i2c_write: pads on bus probably not configured (status=0x10)
Scaling voltage failed for 0x2b
iva: 1099
do_scale_vcore: volt - 1099 offset_code - 0x42
i2c_write: pads on bus probably not configured (status=0x10)
Scaling voltage failed for 0x37
setup_dplls
core Dpll locked, but not for ideal M = 266,N = 4 values, current values are M = 532,N= 9Core DPLL configured
per Dpll locked, but not for ideal M = 96,N = 4 values, current values are M = 1920,N= �NN�Q��DPLL locked
I am using vision sdk 03.04 sdk version.
Could you please help me to solve this issue.
I am unable to write data in to EEPROM.but the chip is detecting at the chip address.
Thanks & Regards,
A.Kavya Harini