Normal 0 false false false EN-US X-NONE HE
Hello
I'm using the TMS320DM6437 EVM, and developing in CCS v3.3 + flashburn DSK v3.11
My project is based on "Accessing_Pixels_In_A_Frame_1_03"
In this project I receive NTSC video and applying some video manipulations (Zoom with the resizer and histogram equalization (HE)) and then output the manipulated video.
The manipulations supposed to be in real time, I checked the processing time and it's less than 30ms per frame).
The problem:
When I'm watching the results in the monitor for +-15 min everything is working great but after that some frames aren't processed, I am starting see flashes of unprocessed frame.
Tried many thing but nothing worked…
Thank you for your time
Shimon akrish