This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5749: About developing Qt application on AM5749

Guru 16800 points

Part Number: AM5749

Hello,

We have two questions about developing Qt application on AM5749.

1.Could you tell us the way to generate executable files by Qt Creator?
  We're referring the following information.
  software-dl.ti.com/.../Examples_and_Demos_Sub-system_Demos.html
  And, Qt Creator generates shared library not executable files.
  We need the way to generate executable files.

2.Is there any way to control GPIO, I2C, SPI from Qt applications?
  We want to control GPIO, I2C, SPI from Qt applications.

The following is the environment.
CPU: AM5749(custom board) (We've confirmed working matrix window normally.)
SDK: ti-processor-sdk-linux-am57xx-evm-06.03.00.106
OS: Ubuntu 18.04 (Qt 5.14.2)

Best Regards,
Nomo