Part Number: AM6546
Other Parts Discussed in Thread: PCA9554
Hi,
I have placed rootfs in second partition of SD card(MMC1). When mounting rootfs from SD card it is failing.Execution stops at "waiting for root device".
I have verified PARTUUID as well, and hard coded bootargs "root=/dev/mmcblk1p2 rw rootfstype=ext4 rootwait",still I am facing same issue.
By observing log i came to know that kernel is not able to detect MMC1 partition,I found some information from below link:

I provided rootdelay in bootargs as well. Still I am facing the same issue.Help me in resolving this issue.
As we are using custom board, i have verified power supply and pin configurations, which are similar to evm.
sdk: PROCESSOR-SDK-LINUX-AM65X 07_00_01_06
processor: am6546 SR 2.0
Please find log below.
U-Boot SPL 2020.01-gf9b0d030d3 (Aug 10 2020 - 17:47:39 +0000) SYSFW ABI: 3.0 (firmware rev 0x0014 '20.04.1-v2020.04a (Terrific Lla') Reading on-board EEPROM at 0x50 failed -1 Trying to boot from MMC2 Starting ATF on ARM64 core... NOTICE: BL31: v2.3():07.00.00.005-dirty NOTICE: BL31: Built : 17:03:45, Aug 10 2020 U-Boot SPL 2020.01-gf9b0d030d3 (Aug 10 2020 - 17:11:07 +0000) SYSFW ABI: 3.0 (firmware rev 0x0014 '20.04.1-v2020.04a (Terrific Lla') Reading on-board EEPROM at 0x50 failed -1 Reading daughtercard EEPROM at 0x55 failed 1 Trying to boot from MMC2 U-Boot 2020.01-dirty (Sep 10 2020 - 13:06:48 +0530) SoC: AM65X SR2.0 Model: Texas Instruments AM654 Base Board Reading on-board EEPROM at 0x50 failed -1 Board: AM6-COMPROCEVM rev E3 DRAM: 4 GiB MMC: sdhci@4f80000: 0, sdhci@04FA0000: 1 Loading Environment from MMC... *** Warning - bad CRC, using default environment In: serial Out: serial Err: serial Reading on-board EEPROM at 0x50 failed -1 Reading daughtercard EEPROM at 0x55 failed 1 Net: Warning: cpsw_nuss@046000000 using MAC address from ROM eth0: cpsw_nuss@046000000 Hit any key to stop autoboot: 0 switch to partitions #0, OK mmc1 is current device SD/MMC found on device 1 1011 bytes read in 6 ms (164.1 KiB/s) Loaded env from uEnv.txt Importing environment from mmc1 ... Running uenvcmd ... 16654344 bytes read in 1332 ms (11.9 MiB/s) 67559 bytes read in 11 ms (5.9 MiB/s) ## Flattened Device Tree blob at 82000000 Booting using the fdt blob at 0x82000000 Loading Device Tree to 00000000fddb1000, end 00000000fdec4fff ... OK Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034] [ 0.000000] Linux version 5.4.40-g66cf445b76 (administrator@administrator-OptiPlex-7010) (gcc version 9.2.1 20191025 (GNU Toolchain for the A-profile Architecture 90 [ 0.000000] Machine model: Texas Instruments AM654 Base Board [ 0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '') [ 0.000000] printk: bootconsole [ns16550a0] enabled [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a0000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0100000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node r5f-memory@a0100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a1000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1100000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node r5f-memory@a1100000, compatible id shared-dma-pool [ 0.000000] cma: Reserved 512 MiB at 0x00000000c0000000 [ 0.000000] psci: probing for conduit method from DT. [ 0.000000] psci: PSCIv1.1 detected in firmware. [ 0.000000] psci: Using standard PSCI v0.2 function IDs [ 0.000000] psci: Trusted OS migration not required [ 0.000000] psci: SMC Calling Convention v1.0 [ 0.000000] percpu: Embedded 2 pages/cpu s48408 r8192 d74472 u131072 [ 0.000000] Detected VIPT I-cache on CPU0 [ 0.000000] CPU features: detected: ARM erratum 845719 [ 0.000000] CPU features: detected: GIC system register CPU interface [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 55976 [ 0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 mtdparts=47040000.spi.0:512k(ospi.tiboot3),2m(ospi.tispl),4m(ospi.u-boott [ 0.000000] Dentry cache hash table entries: 524288 (order: 6, 4194304 bytes, linear) [ 0.000000] Inode-cache hash table entries: 262144 (order: 5, 2097152 bytes, linear) [ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off [ 0.000000] software IO TLB: mapped [mem 0xbbff0000-0xbfff0000] (64MB) [ 0.000000] Memory: 3515712K/3586048K available (9534K kernel code, 776K rwdata, 3840K rodata, 1728K init, 695K bss, 18446744073709097664K reserved, 524288K cma-res) [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1 [ 0.000000] rcu: Preemptible hierarchical RCU implementation. [ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=4. [ 0.000000] Tasks RCU enabled. [ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies. [ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4 [ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0 [ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode [ 0.000000] GICv3: 960 SPIs implemented [ 0.000000] GICv3: 0 Extended SPIs implemented [ 0.000000] GICv3: Distributor has no Range Selector support [ 0.000000] GICv3: 16 PPIs implemented [ 0.000000] GICv3: no VLPI support, no direct LPI support [ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001880000 [ 0.000000] ITS [mem 0x01820000-0x0182ffff] [ 0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS [ 0.000000] ITS@0x0000000001820000: allocated 1048576 Devices @8c0800000 (flat, esz 8, psz 64K, shr 0) [ 0.000000] ITS: using cache flushing for cmd queue [ 0.000000] GICv3: using LPI property table @0x00000008c00d0000 [ 0.000000] GIC: using cache flushing for LPI property table [ 0.000000] GICv3: CPU0: using allocated LPI pending table @0x00000008c00e0000 [ 0.000000] random: get_random_bytes called from start_kernel+0x2b8/0x438 with crng_init=0 [ 0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys). [ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns [ 0.000006] sched_clock: 56 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns [ 0.008642] Console: colour dummy device 80x25 [ 0.013249] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000) [ 0.023969] pid_max: default: 32768 minimum: 301 [ 0.028829] LSM: Security Framework initializing [ 0.033643] Mount-cache hash table entries: 8192 (order: 0, 65536 bytes, linear) [ 0.041253] Mountpoint-cache hash table entries: 8192 (order: 0, 65536 bytes, linear) [ 0.073432] ASID allocator initialised with 32768 entries [ 0.087016] rcu: Hierarchical SRCU implementation. [ 0.100113] Platform MSI: gic-its@1820000 domain created [ 0.105867] PCI/MSI: /interconnect@100000/interrupt-controller@1800000/gic-its@1820000 domain created [ 0.123383] smp: Bringing up secondary CPUs ... [ 0.160645] Detected VIPT I-cache on CPU1 [ 0.160683] GICv3: CPU1: found redistributor 1 region 0:0x00000000018a0000 [ 0.160699] GICv3: CPU1: using allocated LPI pending table @0x00000008c00f0000 [ 0.160749] CPU1: Booted secondary processor 0x0000000001 [0x410fd034] [ 0.192811] Detected VIPT I-cache on CPU2 [ 0.192851] GICv3: CPU2: found redistributor 100 region 0:0x00000000018c0000 [ 0.192867] GICv3: CPU2: using allocated LPI pending table @0x00000008c0100000 [ 0.192917] CPU2: Booted secondary processor 0x0000000100 [0x410fd034] [ 0.224814] Detected VIPT I-cache on CPU3 [ 0.224845] GICv3: CPU3: found redistributor 101 region 0:0x00000000018e0000 [ 0.224859] GICv3: CPU3: using allocated LPI pending table @0x00000008c0110000 [ 0.224897] CPU3: Booted secondary processor 0x0000000101 [0x410fd034] [ 0.225045] smp: Brought up 1 node, 4 CPUs [ 0.305436] SMP: Total of 4 processors activated. [ 0.310271] CPU features: detected: 32-bit EL0 Support [ 0.315567] CPU features: detected: CRC32 instructions [ 0.332336] CPU: All CPU(s) started at EL2 [ 0.336579] alternatives: patching kernel code [ 0.342713] devtmpfs: initialized [ 0.356495] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns [ 0.366522] futex hash table entries: 1024 (order: 0, 65536 bytes, linear) [ 0.375256] pinctrl core: initialized pinctrl subsystem [ 0.381651] NET: Registered protocol family 16 [ 0.393392] DMA: preallocated 256 KiB pool for atomic allocations [ 0.400558] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers. [ 0.430092] HugeTLB registered 16.0 GiB page size, pre-allocated 0 pages [ 0.436999] HugeTLB registered 512 MiB page size, pre-allocated 0 pages [ 0.443803] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages [ 0.456100] cryptd: max_cpu_qlen set to 1000 [ 0.471143] iommu: Default domain type: Translated [ 0.476572] SCSI subsystem initialized [ 0.481046] mc: Linux media interface: v0.10 [ 0.485497] videodev: Linux video capture interface: v2.00 [ 0.491161] pps_core: LinuxPPS API ver. 1 registered [ 0.496259] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it> [ 0.505649] PTP clock support registered [ 0.509699] EDAC MC: Ver: 3.0.0 [ 0.513986] FPGA manager framework [ 0.517566] Advanced Linux Sound Architecture Driver Initialized. [ 0.524872] clocksource: Switched to clocksource arch_sys_counter [ 0.531368] VFS: Disk quotas dquot_6.6.0 [ 0.535518] VFS: Dquot-cache hash table entries: 8192 (order 0, 65536 bytes) [ 0.549394] thermal_sys: Registered thermal governor 'step_wise' [ 0.549399] thermal_sys: Registered thermal governor 'power_allocator' [ 0.556185] NET: Registered protocol family 2 [ 0.567931] tcp_listen_portaddr_hash hash table entries: 4096 (order: 0, 65536 bytes, linear) [ 0.576824] TCP established hash table entries: 32768 (order: 2, 262144 bytes, linear) [ 0.585264] TCP bind hash table entries: 32768 (order: 3, 524288 bytes, linear) [ 0.593443] TCP: Hash tables configured (established 32768 bind 32768) [ 0.600325] UDP hash table entries: 2048 (order: 0, 65536 bytes, linear) [ 0.607326] UDP-Lite hash table entries: 2048 (order: 0, 65536 bytes, linear) [ 0.614968] NET: Registered protocol family 1 [ 0.620254] RPC: Registered named UNIX socket transport module. [ 0.626347] RPC: Registered udp transport module. [ 0.631179] RPC: Registered tcp transport module. [ 0.636010] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.642630] PCI: CLS 0 bytes, default 64 [ 0.647849] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available [ 0.666394] Initialise system trusted keyrings [ 0.671171] workingset: timestamp_bits=46 max_order=16 bucket_order=0 [ 0.684575] squashfs: version 4.0 (2009/01/31) Phillip Lougher [ 0.691409] NFS: Registering the id_resolver key type [ 0.696637] Key type id_resolver registered [ 0.700945] Key type id_legacy registered [ 0.705074] nfs4filelayout_init: NFSv4 File Layout Driver Registering... [ 0.712210] 9p: Installing v9fs 9p2000 file system support [ 0.737964] Key type asymmetric registered [ 0.742188] Asymmetric key parser 'x509' registered [ 0.747247] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 244) [ 0.754843] io scheduler mq-deadline registered [ 0.759494] io scheduler kyber registered [ 0.766227] pinctrl-single 4301c000.pinmux: 70 pins, size 280 [ 0.772733] pinctrl-single 11c000.pinmux: 185 pins, size 740 [ 0.778705] pinctrl-single 11c2e8.pinmux: 9 pins, size 36 [ 0.785494] pinctrl-single a40000.timesync_router: 512 pins, size 2048 [ 0.798365] k3-ringacc 2b800000.ringacc: Failed to get MSI domain [ 0.804741] k3-ringacc 3c000000.ringacc: Failed to get MSI domain [ 0.815236] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled [ 0.839027] brd: module loaded [ 0.851281] loop: module loaded [ 0.858494] libphy: Fixed MDIO Bus: probed [ 0.863279] tun: Universal TUN/TAP device driver, 1.6 [ 0.869275] igbvf: Intel(R) Gigabit Virtual Function Network Driver - version 2.4.0-k [ 0.877318] igbvf: Copyright (c) 2009 - 2012 Intel Corporation. [ 0.883447] sky2: driver version 1.30 [ 0.888428] VFIO - User Level meta-driver version: 0.3 [ 0.894608] i2c /dev entries driver [ 0.899473] sdhci: Secure Digital Host Controller Interface driver [ 0.905824] sdhci: Copyright(c) Pierre Ossman [ 0.910894] sdhci-pltfm: SDHCI platform and OF driver helper [ 0.917964] ledtrig-cpu: registered to indicate activity on CPUs [ 0.924245] ti-sci interconnect@100000:interconnect@28380000:interconnect@42040000:dmsc: invalid resource [ 0.935492] optee: probing for conduit method from DT. [ 0.940826] optee: revision 3.8 (199fca17) [ 0.941653] optee: initialized driver [ 0.951386] NET: Registered protocol family 17 [ 0.956137] 9pnet: Installing 9P2000 support [ 0.960595] Key type dns_resolver registered [ 0.965406] registered taskstats version 1 [ 0.969626] Loading compiled-in X.509 certificates [ 0.983440] k3-ringacc 2b800000.ringacc: Failed to get MSI domain [ 0.989966] k3-ringacc 3c000000.ringacc: Failed to get MSI domain [ 1.001753] ti-sci interconnect@100000:interconnect@28380000:interconnect@42040000:dmsc: invalid resource [ 1.011798] ti-sci interconnect@100000:interconnect@28380000:interconnect@42040000:dmsc: ABI: 3.0 (firmware rev 0x0014 '20.04.1-v2020.04a (Terrific Lla') [ 1.061780] omap_i2c 42120000.i2c: bus 0 rev0.12 at 400 kHz [ 1.068290] omap_i2c 40b00000.i2c: bus 1 rev0.12 at 100 kHz [ 1.074930] pca953x 2-0021: 2-0021 supply vcc not found, using dummy regulator [ 1.105166] random: fast init done [ 1.109080] omap_i2c 2000000.i2c: bus 2 rev0.12 at 400 kHz [ 1.115721] omap_i2c 2010000.i2c: bus 3 rev0.12 at 400 kHz [ 1.122126] omap_i2c 2020000.i2c: bus 4 rev0.12 at 400 kHz [ 1.128417] omap_i2c 2030000.i2c: bus 5 rev0.12 at 100 kHz [ 1.134303] ti-sci-intr interconnect@100000:interconnect@28380000:interconnect@42040000:interrupt-controller2: Interrupt Router 156 domain created [ 1.147983] ti-sci-intr interconnect@100000:interrupt-controller0: Interrupt Router 100 domain created [ 1.157732] ti-sci-intr interconnect@100000:navss@30800000:interrupt-controller1: Interrupt Router 182 domain created [ 1.168948] ti-sci-inta 33d00000.interrupt-controller: Interrupt Aggregator domain 179 created [ 1.185613] k3-ringacc 2b800000.ringacc: Ring Accelerator probed rings:286, gp-rings[96,160] sci-dev-id:195 [ 1.195635] k3-ringacc 2b800000.ringacc: dma-ring-reset-quirk: disabled [ 1.202433] k3-ringacc 2b800000.ringacc: RA Proxy rev. 66348100, num_proxies:64 [ 1.223591] k3-ringacc 3c000000.ringacc: Ring Accelerator probed rings:818, gp-rings[304,464] sci-dev-id:187 [ 1.233736] k3-ringacc 3c000000.ringacc: dma-ring-reset-quirk: disabled [ 1.240535] k3-ringacc 3c000000.ringacc: RA Proxy rev. 66348100, num_proxies:64 [ 1.248659] omap8250 40a00000.serial: PM domain pd:149 will not be powered off [ 1.256498] 40a00000.serial: ttyS1 at MMIO 0x40a00000 (irq = 8, base_baud = 6000000) is a 8250 [ 1.266517] 2800000.serial: ttyS2 at MMIO 0x2800000 (irq = 17, base_baud = 3000000) is a 8250 [ 1.275328] printk: console [ttyS2] enabled [ 1.275328] printk: console [ttyS2] enabled [ 1.283793] printk: bootconsole [ns16550a0] disabled [ 1.283793] printk: bootconsole [ns16550a0] disabled [ 1.294720] 2810000.serial: ttyS3 at MMIO 0x2810000 (irq = 18, base_baud = 3000000) is a 8250 [ 1.304128] 2820000.serial: ttyS4 at MMIO 0x2820000 (irq = 19, base_baud = 3000000) is a 8250 [ 1.316239] cadence-qspi 47040000.spi: mt35xu512aba (65536 Kbytes) [ 1.322452] 7 cmdlinepart partitions found on MTD device 47040000.spi.0 [ 1.329068] Creating 7 MTD partitions on "47040000.spi.0": [ 1.334561] 0x000000000000-0x000000080000 : "ospi.tiboot3" [ 1.341576] 0x000000080000-0x000000280000 : "ospi.tispl" [ 1.348160] 0x000000280000-0x000000680000 : "ospi.u-boot" [ 1.354929] 0x000000680000-0x0000006a0000 : "ospi.env" [ 1.361481] 0x0000006a0000-0x0000006c0000 : "ospi.env.backup" [ 1.368502] 0x0000006c0000-0x0000007c0000 : "ospi.sysfw" [ 1.375294] 0x000000800000-0x000004000000 : "ospi.rootfs" [ 1.605630] cadence-qspi 47040000.spi: Cadence QSPI NOR probe failed -517 [ 1.660890] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 1000000 [ 1.668563] libphy: 46000f00.mdio: probed [ 1.674055] davinci_mdio 46000f00.mdio: phy[0]: device 46000f00.mdio:00, driver TI DP83867 [ 1.682365] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA00102, cpsw version 0x6BA80102 Ports: 2 [ 1.693910] am65-cpsw-nuss 46000000.ethernet: Failed to request tx dma channel -517 [ 1.703676] am65-cpts 310d0000.cpts: CPTS ver 0x4e8a010b, freq:200000000, add_val:4 pps:0 [ 1.713298] mmc0: CQHCI version 5.10 [ 1.748123] mmc0: SDHCI controller on 4f80000.sdhci [4f80000.sdhci] using ADMA 64-bit [ 1.768472] pca953x 0-0039: 0-0039 supply vcc not found, using dummy regulator [ 1.796928] pca953x 0-0039: failed writing register [ 1.801968] pca953x: probe of 0-0039 failed with error -121 [ 1.811596] ti-udma 285c0000.dma-controller: Channels: 96 (tchan: 48, rchan: 48, gp-rflow: 48) [ 1.834996] ti-udma 31150000.dma-controller: Channels: 267 (tchan: 119, rchan: 148, gp-rflow: 150) [ 1.850006] mmc0: Command Queue Engine enabled [ 1.854482] mmc0: new HS200 MMC card at address 0001 [ 1.869764] mmcblk0: mmc0:0001 S0J57X 29.6 GiB [ 1.874625] mmcblk0boot0: mmc0:0001 S0J57X partition 1 31.5 MiB [ 1.881678] mmcblk0boot1: mmc0:0001 S0J57X partition 2 31.5 MiB [ 1.887915] mmcblk0rpmb: mmc0:0001 S0J57X partition 3 4.00 MiB, chardev (240:0) [ 1.897398] cadence-qspi 47040000.spi: mt35xu512aba (65536 Kbytes) [ 1.903589] 7 cmdlinepart partitions found on MTD device 47040000.spi.0 [ 1.910569] Creating 7 MTD partitions on "47040000.spi.0": [ 1.916363] 0x000000000000-0x000000080000 : "ospi.tiboot3" [ 1.923350] 0x000000080000-0x000000280000 : "ospi.tispl" [ 1.932722] 0x000000280000-0x000000680000 : "ospi.u-boot" [ 1.939413] 0x000000680000-0x0000006a0000 : "ospi.env" [ 1.945964] 0x0000006a0000-0x0000006c0000 : "ospi.env.backup" [ 1.953199] 0x0000006c0000-0x0000007c0000 : "ospi.sysfw" [ 1.959866] 0x000000800000-0x000004000000 : "ospi.rootfs" [ 1.973312] spi-nor spi7.0: unrecognized JEDEC id bytes: 00 00 00 00 00 00 [ 1.980228] spi-nor: probe of spi7.0 failed with error -2 [ 2.024901] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 1000000 [ 2.032567] libphy: 46000f00.mdio: probed [ 2.038052] davinci_mdio 46000f00.mdio: phy[0]: device 46000f00.mdio:00, driver TI DP83867 [ 2.046366] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA00102, cpsw version 0x6BA80102 Ports: 2 [ 2.059101] am65-cpsw-nuss 46000000.ethernet: set new flow-id-base 48 [ 2.067095] pps pps0: new PPS source ptp1 [ 2.071458] am65-cpsw-nuss 46000000.ethernet: CPTS ver 0x4e8a010b, freq:200000000, add_val:4 pps:1 [ 2.080430] am65-cpsw-nuss 46000000.ethernet: initialized cpsw ale version 57.4 [ 2.087738] am65-cpsw-nuss 46000000.ethernet: ALE Table size 64 [ 2.098359] debugfs: Directory 'pd:121' with parent 'pm_genpd' already present! [ 2.105728] debugfs: Directory 'pd:120' with parent 'pm_genpd' already present! [ 2.115296] input: gpio-keys as /devices/platform/gpio-keys/input/input0 [ 2.123101] hctosys: unable to open rtc device (rtc0) [ 2.138309] ALSA device list: [ 2.141350] No soundcards found. [ 2.145249] Waiting 5 sec before mounting root device... [ 7.237068] Waiting for root devic
Regards,
N Chetan Kumar