Hi,
My software version: visionSDK3.08.
When I make a boot sd card, the drm crash log appears when it first starts.
In order to reproduce this phenomenon, I put avm_qt_app in front of apps.out to start, and then this kind of crash almost became a phenomenon(9/10) .
Is the control screen too early to cause the abnormal phenomenon?
The crash log is as follows:
Arago 2019.09 dra7xx-evm ttyS0
dra7xx-evm login: [ 17.976754] ------------[ cut here ]------------
[ 17.982396] WARNING: CPU: 1 PID: 55 at drivers/gpu/drm/drm_atomic_helper.c:1386 drm_atomic_helper_wait_for_vblanks.part.1+0x290/0x298
[ 17.996997] [CRTC:31:crtc-0] vblank wait timed out
[ 18.001865] Modules linked in: ax88179_178a extcon_usb_gpio cdc_ether usbnet c_can_platform r8152 ahci_platform c_can libahci_platform libahci can_dev xhci_plat_hcd omap_sham xhci_hcd omap_aes_driver usbcore libata phy_omap_usb2 dwc3 udc_core omap_des usb_common des_generic dwc3_omap omap_hdq rtc_omap crypto_engine wire omap_crypto sch_fq_codel vmouse(O) cmemk(O) memcache(O) rpmsg_rpc rpmsg_proto omap_remoteproc virtio_rpmsg_bus remoteproc pvrsrvkm(O)
[ 18.044930] CPU: 1 PID: 55 Comm: kworker/u4:1 Tainted: G O 4.19.73 #3
[ 18.052708] Hardware name: Generic DRA74X (Flattened Device Tree)
[ 18.058836] Workqueue: events_unbound commit_work
[ 18.063564] Backtrace:
[ 18.066033] [<c020cad4>] (dump_backtrace) from [<c020ce0c>] (show_stack+0x18/0x1c)
[ 18.073638] r7:c0e15988 r6:60030013 r5:00000000 r4:c1251df0
[ 18.079330] [<c020cdf4>] (show_stack) from [<c09fdf40>] (dump_stack+0x90/0xa4)
[ 18.086590] [<c09fdeb0>] (dump_stack) from [<c0231f80>] (__warn+0xdc/0xf8)
[ 18.093496] r7:c0e15988 r6:00000009 r5:00000000 r4:eea85e24
[ 18.099182] [<c0231ea4>] (__warn) from [<c0231bc4>] (warn_slowpath_fmt+0x50/0x6c)
[ 18.106700] r9:00000001 r8:00000000 r7:00000000 r6:000002d0 r5:c0e15bf0 r4:c1204c48
[ 18.114480] [<c0231b78>] (warn_slowpath_fmt) from [<c063d538>] (drm_atomic_helper_wait_for_vblanks.part.1+0x290/0x298)
[ 18.125222] r3:0000001f r2:c0e15bf0
[ 18.128812] r5:00000000 r4:ee4f7000
[ 18.132405] [<c063d2a8>] (drm_atomic_helper_wait_for_vblanks.part.1) from [<c063f024>] (drm_atomic_helper_commit_tail+0x64/0x74)
[ 18.144020] r10:00000000 r9:d7fa0c30 r8:00000000 r7:ef005000 r6:ef006200 r5:ee5f0800
[ 18.151883] r4:d7fa0c00
[ 18.154431] [<c063efc0>] (drm_atomic_helper_commit_tail) from [<c063f0a4>] (commit_tail+0x70/0x74)
[ 18.163428] r5:00000000 r4:d7fa0c00
[ 18.167021] [<c063f034>] (commit_tail) from [<c063f0bc>] (commit_work+0x14/0x18)
[ 18.174449] r5:ef0d1180 r4:d7fa0c2c
[ 18.178044] [<c063f0a8>] (commit_work) from [<c0249f98>] (process_one_work+0x1f4/0x404)
[ 18.186087] [<c0249da4>] (process_one_work) from [<c024ad58>] (worker_thread+0x58/0x568)
[ 18.194215] r10:ef006200 r9:c1203d00 r8:ef006218 r7:00000088 r6:ef006200 r5:ef0d1194
[ 18.202077] r4:ef0d1180
[ 18.204627] [<c024ad00>] (worker_thread) from [<c0250238>] (kthread+0x160/0x168)
[ 18.212058] r10:ef0a1e74 r9:c024ad00 r8:ef0d1180 r7:eea84000 r6:00000000 r5:ef0ce840
[ 18.219921] r4:eea75f80
[ 18.222469] [<c02500d8>] (kthread) from [<c02010d8>] (ret_from_fork+0x14/0x3c)
[ 18.229723] Exception stack(0xeea85fb0 to 0xeea85ff8)
[ 18.234796] 5fa0: 00000000 00000000 00000000 00000000
[ 18.243009] 5fc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 18.251222] 5fe0: 00000000 00000000 00000000 00000000 00000013 00000000
[ 18.257867] r10:00000000 r9:00000000 r8:00000000 r7:00000000 r6:00000000 r5:c02500d8
[ 18.265729] r4:ef0ce840
[ 18.271615] ---[ end trace 2b55ac1458174ae3 ]---