This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-AM335X: NAND flashing through UART

Part Number: PROCESSOR-SDK-AM335X
Other Parts Discussed in Thread: AM3358, UNIFLASH

Hi!

I am using sitara AM3358 processor on custom board with RTOS SDK 6_01_00_08. 

I have configured NAND Flash Writer as per our NAND. Currently I am flashing the NAND through XDS 110 in debug mode running the NAND flash writer. In this scenario processor is reading binary file through xds 110 available on PC as per given path. Now I want to flash the code through UART. What is the procedure for this? How the processor will read the binary file from my PC?

Regards,

Gaurav