Part Number: TDA4VMXEVM
HI.master
We have executed: UFS utils desc - t 1 - W config_ desc_ data_ ind_ 0 -p /dev/bsg/ufs-bsg0
However, the UFS device has not been scanned, and the detailed log is in the file.
SDK:ti-processor-sdk-linux-automotive-j7-evm-07_00_00
[11:04:12]Hit any key to stop autoboot: 0
[11:04:13]=>
[11:04:13]=>
[11:04:19]=>
[11:04:20]=>
[11:04:24]=> ufs init
[11:04:24]Device at ufs@4e84000 up at:[RX, TX]: gear=[3, 3], lane[2, 2], pwr[FAST MODE, FAST MODE], rate = 2
[11:04:29]=> scsi scan
[11:04:29]scanning bus for devices...
[11:04:31]=>
[11:04:31]scanning bus for devices...
[11:04:31]=>
....
]root@j7-evm:~# ufs-utils desc -t 1 -w config_desc_data_ind_0 -p /dev/bsg/ufs-bsg0
[11:06:36]Config Descriptor was written to device
[11:06:44]root@j7-evm:~# [ 129.093570] Initializing XFRM netlink socket
[11:06:47][ 132.610765] bridge: filtering via arp/ip/ip6tables is no longer available by default. Update your scripts to load br_netfilter if you need this.
[11:06:47][ 132.629016] Bridge firewalling registered
[11:08:02]root@j7-evm:~#
[11:08:05]root@j7-evm:~# ls /dev/s
[11:08:05]shm/ snapshot snd/ stderr stdin stdout
[11:08:07]root@j7-evm:~# ls /dev/s