Part Number: OMAP-L138
Other Parts Discussed in Thread: OMAPL138,
We're interfacing to the MT47H64M16NF, no serial termination resistors, DVDD = 1.8V (no termination due to space constraints). We see 2.44V of overshoot for about 21% of the period and slight undershoot that does not go below 1.8V - 0.3V. We also see negative overshoot (below 0V) to -460mV for about 17% of the period. This is a Hyperlynx simulation using sprm378c/omapl138_zwt.ibs, fast-strong case and the DDR is set to "DQ_HALF_800" drive. We noticed this ibis has no input model so we used the Output Tri-State (DQ_NOSR0_NOTERM_0).
1. Is this voltage waveform within the absolute maximum limits?
2. Is the Absolute Maximum Clamp Current at +/-20mA measured at DVDD + 0.3V? Is our voltage waveform going to result in a clamp current of >20mA when it drifts above DVDD+0.3V?
3. Ibis model POWER Clamp is ~3mA at -540mV (1.9V - 2.44V). We see this current in the simulation, after the rising edge dv/dt spike. Why is this current much less than the 20mA above?