Hi all,
I'm starting to work with OMAP4 Blaze.
I have a problem to connect the board to HyperTerminal.
My OMAP4 (SEVM4430G-00-01-00) have only one config CTL - S2 tag. I configure it: 1 - OFF, 2,3,4 - ON.
After connection the board to Windows PC In Device Manager USB controller added for additional entries (USB Serial Converted A,B,C,D) and under Ports (COM and LPT)
added 4 USB Serial ports(18,19,20,21)
I tried to configure the HyperTerminal with 18,19,20,21 ports.
Other HyperTerminal configurations: (BitRate=18115200, DataBits=8, Parity=None, StopBits=1, FlowControl=None)
My Board have Reset Button near the Ethernet entry, i'm not if its work properly.
I did the reset by dissconnect/connect power cable.
I can't see any response from the board via HyperTerminal.
Please assist to fix the problem.
BR
Evgeny