Part Number: TDA4VM
Hi TI members,
We are using PSDKLA 06.02.
On our custom board, we connect USB0 to an M.2 connector, and SERDES1_LANE1 to another M.2 connector.
Here are some questions:
1. Is there any command (e.g. devmem2) that can set USB 2.0 host (USB0) to test mode in linux?
I cannot find related register in TRM.
2. During compliance test, there is no CP0 or CP1 from the M.2 connector connected to USB 3.0 host (SERDES1_LANE1).
After connecting M.2 to our test fixture, since USB 3.0 host cannot detect any USB 3.0 device, shouldn't it enter compliance mode and start to generate CP0?
Best regards,
Eric Chen