This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM365_Edge enhancement function Problem

Dear All,

I try to implement  Edge enhancement(EE) module  in DM365_IPIPE.

But, strangely, when i set  EE enable register, DM365_IPIPE Block is died (non-opration) and it's possible only image capture.

 I tried to access kernel(by dm365_def_para.c) or direct register setting (IPIPE_YEE)  for  EE enable method.

but result is the same thing.(failed)

My system data flow is as blow. (that is one-shot mode)

Raw sensor -> IPIPEIF -> ISIF -> SDRAM -> IPIPEIF -> IPIPE -> SDRAM -> RESIZE(IPIPE-passthrough) -> Codec

I refer to dvsdk_xxx\ PSP_02_10_00_14\examples\dm365\previewer_resizer\do_preview_resize.c and applied EE register values.

EE LUT is same EE_Table.txt.

Pls help me how to slove this problem..