This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
SDK: ti-processor-sdk-linux-am335x-evm-06.03.00.106
bootmode: 00010b URAT0 -> SPI0 -> NAND->NANDI2C;
When custom board booting (MLO and u-boot.img ) from Nand, it will automatically restart
When booting (u-boot-spl.bin and u-boot.img) from UART, it boots normally and and can execute uboot command.
Comparing MLO and u-boot-spl.bin, there is an extra GP header.
Below is output:
CCCCCCCC
U-Boot SPL 2019.01-g7339be8-dirty (Sep 17 2020 - 15:58:18 +0800)
Trying to boot from NAND
U-Boot 2019.01-g7339be8-dirty (Sep 17 2020 - 15:58:18 +0800)
CPU : AM335X-GP rev 2.1
Model: TI AM335x EVM
DRAM: 512 MiB
NAND: 256 MiB
MMC: OMAP SD/MMC: 0
Loading Environment from FAT... <ethaddr> not set. Validating first E-fuse MAC
Net: eth0: ethernet@4a100000
Warning: usb_ether MAC addresses don't match:
Address in ROM is de:ad:be:ef:00:01
Address in environment is f8:30:02:e5:a6:77
, eth1: usb_ether
Hit any key to stop autoboot: 2 CCCCCCCC
Hi Nancy,
I tested with MLO & u-boot.img built from SDK 6.3 on TI GP EVM, and no issue was observed for nand booting.
Would you be able to stop @u-boot prompt on your nand booting setup?
Best,
-Hong
Hi,
No, it cannot stop at uboot prompt.
Will the watchdog be turned on when device booting?
Hi Nancy,
Yes, WDT is turned on in u-boot when booting.
I tested on TI AM335x GP EVM with SDK 6.3, and no issue was observed on 1/. nand flashing from mmc boot, and 2/. nand booting afterwards.
Best,
-Hong
Hi,
It was found that the external watchdog caused the restart. Watchdog is temporarily removed, nand can boot normally. What will affect the pins of watchdog?
Hi Nancy,
For debugging purpose, one option to disable HW_WDT in AM335x SPL/u-boot is to commenting off hw_watchdog_init() in /arch/arm/mach-omap2/boot-common.c as listed below:
#if defined(CONFIG_HW_WATCHDOG) // hw_watchdog_init(); #endif
Please refer to Section 20.4 for details on WDT in AM335x TRM ()
Best,
-Hong