Part Number: TDA4VMXEVM
Hi team,
is it possible to run dss_display_test in J721E EVM with a video ?
it's very limited if we can load only YUV files and not JPEG, JPG, PNG or even a video.
Thanks,
Brahim
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TDA4VMXEVM
Hi team,
is it possible to run dss_display_test in J721E EVM with a video ?
it's very limited if we can load only YUV files and not JPEG, JPG, PNG or even a video.
Thanks,
Brahim
Brahim,
Not at the PDK/driver level, but if you are using SDK, then you could use decoder node and can decode H.264 stream and then it can be displayed.
PDK example supports just RAW RGB/YUV formats.
Rgds,
Brijesh
Hi Brijesh,
Do you mean using PSDKRA and booting from SD Card?
Regards,
Brahim