Part Number: TDA4VMXEVM
Hi,
there is some really good documentation for the J7ES EVM PCIe EP mode test with a second J7 EVM in RC mode.
A customer is is trying to configure the J7 PCIe EP mode correctly based on these instructions and then is using the second J7 EVM in PCIe RC mode. However after powering up the J7 EP, and subsequently the J7 RC, the EP does not seem to be enumerated.
Here are the logs:
EP side:
root@j7-evm-ep:/sys/kernel/config/pci_ep# lspci
00:00.0 Class 0604: 104c:b00d
00:00.0 Class 0604: 104c:b00d
root@j7-evm-ep:/sys/kernel/config/pci_ep# cat functions/pci
pci-epf-ntb/ pci_epf_test/
root@j7-evm-ep:/sys/kernel/config/pci_ep# cat functions/pci_epf_test/func1/
baseclass_code deviceid msi_interrupts progif_code subclass_code subsys_vendor_id
cache_line_size interrupt_pin msix_interrupts revid subsys_id vendorid
root@j7-evm-ep:/sys/kernel/config/pci_ep# cat functions/pci_epf_test/func1/vendorid
0x104c
root@j7-evm-ep:/sys/kernel/config/pci_ep# cat functions/pci_epf_test/func1/deviceid
0xb00d
root@j7-evm-ep:/sys/kernel/config/pci_ep# cat functions/pci_epf_test/func1/msi_interrupts
2
root@j7-evm-ep:/sys/kernel/config/pci_ep# cat functions/pci_epf_test/func1/msix_interrupts
2
root@j7-evm-ep:/sys/kernel/config/pci_ep# ls -l controllers/2900000.pcie-ep/
total 0
lrwxrwxrwx 1 root root 0 Sep 20 23:48 func1 -> ../../../pci_ep/functions/pci_epf_test/func1
-rw-r--r-- 1 root root 65536 Sep 20 23:49 start
root@j7-evm-ep:/sys/kernel/config/pci_ep# cat controllers/2900000.pcie-ep/start
1
RC side:
root@j7-evm-rc:~# ls /sys/kernel/config/pci_ep/controllers/
root@j7-evm-rc:~#
root@j7-evm-rc:~# lspci
00:00.0 Class 0604: 104c:b00d
00:00.0 Class 0604: 104c:b00d
00:00.0 Class 0604: 104c:b00d
root@j7-evm-rc:~# ls /dev/pc*
ls: /dev/pc*: No such file or directory
Could you review this and let me know where to look here? Could you confirm the Switch settings for both J7 RC and J7 EP EVMs?
We will double-check everything.
Thanks!
--Gunter