Hi,
I am booting multiple 6474s with an EMAC boot across multiple boards on the same network and I would like to specify the destination MAC address of the BOOTP. Currently the BOOTP packet is broadcast and I would like to specify an exact MAC address for the BOOTP. I can specify the source MAC address but the desination address doesn't take. I modify the EMAC boot parameter structure Host MAC and it doesn't work.
Is changing the destination MAC address of the BOOTP packet supported in the 6474 bootloader?
Thanks
Nick