This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM4376: How to use MPU_RAM by CPDMA

Part Number: AM4376


Hi,

I posted in the following thread about the internal memory settings for the receive descriptor and received a comment that it can be used if it is 0x402F_0400 - 0x402F_FFFF. 
However, My customer says that the 0x402F_0400 - 0x402F_FFFF region will not write any incoming data at all. This area is not used by the OS.
The 0x4030_0000 in the OCMCRAM region is not a problem.

Do We need to do any special configuration to use MPU_RAM(0x402F_0400 - 0x402F_FFFF)? 


Best Regards,
H.U