This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP-L138 + BOOT + AISGen + Pinmux??

Guru 15580 points

I just wanted to verify that I *do not* need to set the pinmux for the BOOT[0:7] pins in AISGen to boot from SPI flash...? From what I can decipher from the docs, the bootloader latches BOOT[0:7] on the rising edge of Reset regardless of the state of PINMUX17&18....?

Thx,

MikeH