This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-AM335X: SDK release for Dunfell

Part Number: PROCESSOR-SDK-AM335X


Hello,

If I am correct the current Linux Processor SDK release for AM335X available is 06_03_00_106

which appears to based upon Yocto Thud.

1) Will there be a SDK release available in near future based upon Yocto Dunfell? Or is there some timeline / roadmap available for upcoming SDK releases?

Looking into the repos for meta-ti and meta-arago I observed tags like 07.01.00.001 available on dunfell branch. 

2) How should these tags be interpreted? For example stable or working baseline?

Kind regards,

Andre

  • Hi and thanks for your post.

    Andre Hoffard34 said:

    If I am correct the current Linux Processor SDK release for AM335X available is 06_03_00_106

    which appears to based upon Yocto Thud.

    That's correct.

    Andre Hoffard34 said:

    1) Will there be a SDK release available in near future based upon Yocto Dunfell? Or is there some timeline / roadmap available for upcoming SDK releases?

    Looking into the repos for meta-ti and meta-arago I observed tags like 07.01.00.001 available on dunfell branch. 

    We plan to release 7.01 in the late October/early November timeframe and it is based on dunfell branch.

    Andre Hoffard34 said:
    2) How should these tags be interpreted? For example stable or working baseline?

    Until the time of release, these are a working baseline.

    I hope this addresses your questions well. Have a great day.

  • Thanks for info!