Other Parts Discussed in Thread: AM6548
Hello.
We are evaluating AM65xx processors for our next project.
For this purpose we've ordered TMDX654IDKEVM.
As we can see this board contains a heatsink for CPU.
The heatsink is incompatible with our end equipment dimensions.
We are not going to use GPU core of the device.
So the questions are:
1) is it allowed to use AM65xx processors without an external heatsink?
2) what is the maximum operation load level of AM65xx, when there is no requirement to use an external heatsink (in terms of CPU load or utilizing of internal modules)?