Part Number: AM3352
Hi
I use am3352 in my custom board, based on the beaglebone black.
I have a SD card connected to MMC0, the same as BBB.
However, I use different pin for card detection.
BBB uses GPIO0_6, and I use GPIO3_14.
I've created the pinmux configuration using PINMUX TOOL.
Assuming I use the same .dts file structure as BBB, where should I change this pin definition.
I've tried to temporarly change the am335x-bone-common.dtsi
0x160 (PIN_INPUT | MUX_MODE7) /* GPIO0_6 */
AM33XX_IOPAD(0x990, PIN_INPUT | MUX_MODE4) /* (A13) mcasp0_aclkx.mmc0_sdcd */
Unfortunately, I get the same error.
*** Warning - No MMC card found
Where should I change the pin definition?
Moreover, I've found the difference in pin definition in .dts files from u-boot GIT and from PINMUX TOOL.
0x160 (PIN_INPUT | MUX_MODE7) /* GPIO0_6 */
AM33XX_IOPAD(0x990, PIN_INPUT | MUX_MODE4) /* (A13) mcasp0_aclkx.mmc0_sdcd */
Are both these definiotions valid?