Other Parts Discussed in Thread: TMS320F28069
Hi guys!
This is Mike
After learning to use C2000 doing a meter (thanks for those who helped on that) . Now I want to make a meter-logger which can send the data through a Serial-port and in future through the cloud (IoT services). But See this, I have read the ARM is so good for communication but it is just a processor. So I don't if it is a good idea to work with TMS320F28069 and the TMS320C6655, one just for ADC and getting the data and make the calculus, and the TMS320C6655 for sending the data.
Am I wrong or I can use som Hercules (ARM Cortex with ADC integrated but no FPU or DMA) to make the job
I will read threephase systems with variable frequency through DC to 100 Hz
What do you think guys?