Other Parts Discussed in Thread: DM3730, ADS7846
Hi Everyone,
We have a dm3730 based board.
For touch screen interrupt we are using gpio183.
After keeping idle for some time my board is going to suspend mode .
Based on the touch event, the board is not going to wake up.
I have configured the PADCONFIG register to wakeup enable [0x480021C0]
I have done the interrupt configuration on falling edge detect and wake enable in GPIO chapter...
The wake UP is on the PER module, I have configured this also...
I am not able to find the difference between table 13.6 and table 13.4 in DM3730 TRM....
Only the gpios mentioned in table 13.6 are capable of providing wake up in the suspend mode.
Thanks & Regards
ANIL