[ 9.842001] ------------[ cut here ]------------ [ 9.842015] WARNING: CPU: 0 PID: 1 at drivers/bus/omap_l3_noc.c:147 l3_interrupt_handler+0x25c/0x368() [ 9.842021] 44000000.ocp:L3 Standard Error: MASTER PRUSS2 PRU2 TARGET GPMC (Read Link): At Address: 0x40002AAC : Data Access in User mode during Functional access [ 9.842100] Modules linked in: prueth virtio_rpmsg_bus(+) ecb pru_rproc sha512_generic sha512_arm pruss_intc sha256_generic hmac md5 sha1_generic sha1_arm_neon sha1_arm omap_aes_driver c_can_platform c_can pruss can_dev omap_shl [ 9.842107] CPU: 0 PID: 1 Comm: systemd Not tainted 4.4.19-g891425d-dirty #182 [ 9.842110] Hardware name: Generic DRA74X (Flattened Device Tree) [ 9.842114] Backtrace: [ 9.842133] [<c00130e4>] (dump_backtrace) from [<c00132e0>] (show_stack+0x18/0x1c) [ 9.842145] r7:c02dfa98 r6:20010193 r5:00000000 r4:c09f2f8c [ 9.842157] [<c00132c8>] (show_stack) from [<c02b37cc>] (dump_stack+0x8c/0xa0) [ 9.842170] [<c02b3740>] (dump_stack) from [<c0034920>] (warn_slowpath_common+0x88/0xb8) [ 9.842180] r7:c02dfa98 r6:00000093 r5:00000009 r4:ee88dbc8 [ 9.842190] [<c0034898>] (warn_slowpath_common) from [<c0034988>] (warn_slowpath_fmt+0x38/0x40) [ 9.842200] r8:00000017 r7:c08c41e4 r6:00000004 r5:c08c3d80 r4:c08c3e30 [ 9.842209] [<c0034954>] (warn_slowpath_fmt) from [<c02dfa98>] (l3_interrupt_handler+0x25c/0x368) [ 9.842215] r3:ee9fdd80 r2:c08c3e30 [ 9.842219] r4:80080001 [ 9.842228] [<c02df83c>] (l3_interrupt_handler) from [<c007fe60>] (handle_irq_event_percpu+0xb4/0x160) [ 9.842241] r10:c0a26a72 r9:ee9fa840 r8:00000017 r7:00000000 r6:00000000 r5:ee9fa8a0 [ 9.842244] r4:eea03280 [ 9.842253] [<c007fdac>] (handle_irq_event_percpu) from [<c007ff4c>] (handle_irq_event+0x40/0x64) [ 9.842264] r10:00000000 r9:00000000 r8:ee808000 r7:00000000 r6:c09cdec4 r5:ee9fa8a0 [ 9.842267] r4:ee9fa840 [ 9.842276] [<c007ff0c>] (handle_irq_event) from [<c0083278>] (handle_fasteoi_irq+0xc0/0x194) [ 9.842285] r7:00000000 r6:c09cdec4 r5:ee9fa8a0 r4:ee9fa840 [ 9.842293] [<c00831b8>] (handle_fasteoi_irq) from [<c007f48c>] (generic_handle_irq+0x2c/0x3c) [ 9.842302] r7:00000000 r6:00000000 r5:00000017 r4:c09c1424 [ 9.842310] [<c007f460>] (generic_handle_irq) from [<c007f764>] (__handle_domain_irq+0x64/0xbc) [ 9.842318] [<c007f700>] (__handle_domain_irq) from [<c000948c>] (gic_handle_irq+0x40/0x7c) [ 9.842328] r9:00000000 r8:fa213000 r7:fa212000 r6:ee88dd88 r5:fa21200c r4:c09c88e0 [ 9.842334] [<c000944c>] (gic_handle_irq) from [<c0013dc0>] (__irq_svc+0x40/0x74) [ 9.842337] Exception stack(0xee88dd88 to 0xee88ddd0) [ 9.842343] dd80: ee518990 00000002 ee88de38 c09e0360 ee88de50 ee333010 [ 9.842349] dda0: 00000040 00000000 ee88df10 00000000 00000000 ee88ddec 0000000a ee88dddc [ 9.842353] ddc0: c09e0374 c0128048 60010013 ffffffff [ 9.842363] r9:00000000 r8:ee88df10 r7:ee88ddbc r6:ffffffff r5:60010013 r4:c0128048 [ 9.842375] [<c0127fec>] (set_root_rcu) from [<c012a20c>] (path_init+0x204/0x358) [ 9.842379] r4:ee88de38 [ 9.842388] [<c012a008>] (path_init) from [<c012bb20>] (path_lookupat+0x18/0x10c) [ 9.842399] r9:00000000 r8:ee88df10 r7:00000000 r6:ee88df10 r5:ee333000 r4:ee88de38 [ 9.842408] [<c012bb08>] (path_lookupat) from [<c012d4ec>] (filename_lookup+0x98/0xf4) [ 9.842417] r7:00000000 r6:ee88de38 r5:ee333000 r4:00000000 [ 9.842425] [<c012d454>] (filename_lookup) from [<c012d61c>] (user_path_at_empty+0x4c/0x54) [ 9.842435] r8:ee88df40 r7:7f7b9240 r6:ee88df10 r5:ffffff9c r4:00000000 [ 9.842442] [<c012d5d0>] (user_path_at_empty) from [<c0123bc0>] (vfs_fstatat+0x54/0xa8) [ 9.842449] r6:ffffff9c r5:00000000 r4:bee9c6c8 [ 9.842456] [<c0123b6c>] (vfs_fstatat) from [<c0124214>] (SyS_lstat64+0x28/0x44) [ 9.842466] r9:ee88c000 r8:c000fbc4 r7:000000c4 r6:7f7ba240 r5:7f7b9282 r4:bee9c6c8 [ 9.842474] [<c01241ec>] (SyS_lstat64) from [<c000fa20>] (ret_fast_syscall+0x0/0x34) [ 9.842478] r4:7f739c7a [ 9.842481] ---[ end trace 187b46b13c976021 ]---
What could be the cause?