I need to create a new C6713B project in CCS v4.2.1 for an existing custom board, and I can't figure out how to include DSP/BIOS or SYS/BIOS. The Wiki example shows how to enable DSP/BIOS 5 in CCS v4.0, but that option is not present on the newer CCS version 4.2.1. I tried creating a project with SYS/BIOS, but when I compiled a sample project, I got an error message saying "Error: Target not supported: ti.targets.C67 ".
What BIOS version is compatible with the C6713B and CCSv4.2.1, and what must I do to create a project including it?