I am trying to implement sleep on DM355 using DVSDK 3.1. I have found some code here:
http://www.mail-archive.com/davinci-linux-open-source@linux.davincidsp.com/msg04407.html
I had to clean it up a bit. However, there seems to be a problem with DVSDK 3.1.
To put the board to sleep I run: echo "standby" > /sys/power/state
If my understanding is correct, before calling "my" (not actually, I took it from the link above) code, the kernel attempts to notify the drivers about a pending suspend command. The problem is appears with drivers/media/video/davinci_display.c.This driver has one standalone structure (in my case located at address 0xC02AB188):
| file: drivers/media/video/davinci_display.c |
| static struct device_driver davinci_driver = { .name = DAVINCI_DISPLAY_DRIVER, .bus = &platform_bus_type, .probe = davinci_probe, .remove = davinci_remove, }; |
However the kernel is trying to find a parent of this structure and call a pointer located in the parent:
| file: drivers/base/platform.c |
| static int platform_legacy_suspend(struct device *dev, pm_message_t mesg) { struct platform_driver *pdrv = to_platform_driver(dev->driver); struct platform_device *pdev = to_platform_device(dev); int ret = 0; if (dev->driver && pdrv->suspend) ret = pdrv->suspend(pdev, mesg); return ret; } |
In this platform_legacy_suspend function dev->driver points (address 0xC02AB188) to the structure defined above in davinci_display.c.
However the first line in the function is trying to find a container of struct device_driver as if davinci_display.c had it defined as following:
|
static struct platform_driver some_name { |
Since the parent (container of struct device_driver) does not exist, the first line in platform_legacy_suspend() produced a pointer (address 0xC02AB174) outside of the structure.
Now, .suspend field in this non-existing structure contains some garbage data which is interpreted as a pointer to a suspend function (address is 0x000CA800). Obviously this is invalid address for a function and the kernel gives an Oops.
What is going on here? Is the driver structure defined incorrectly?
Thank you.