Hello,
We have been using the Logic PD L138 EVM kit to port/develop some code using the C6748 SOM that Logic had at the time which had an experimental TMX320C6748ZCE, revision-1, 300MHz. CPU. We are looking to create some hardware now and need to zero-in on the right model.
We are not a high-volume user so we need to make sure we choose a model that will be readily available from most distributors.
Questions:
1) So far it seems the ZWT (0.8mm Ball Pitch) version is somewhat more available than the ZCE (0.65mm). Is ZWT more likely to be the main device type? So long as form and function are the same as the ZCE this is fine and is easier to layout.
2) I see that the 'B' (revision 2) seems available. Should I assume that 'A' will no longer be made?
3) In the same thought I see that speed grade 3 for revision 2 is 375MHz rather than 300MHz and that there is a speed grade 4 (456MHz). Assuming that the power increase is mostly proportional with the clock speed, we may be interested in the 456MHz if the design from the original Logic PD EVM boards can still be used as a reference?
4) It seems that the speed grade 3 (375MHz for rev 2) is somewhat available while grade 4 (456MHz) does not seem available . Should I expect that grade 3 will be the primary device and grade 4 a special? Or will grade 4 likely replace grade 3?
Thank you on behalf your small-to-medium-volume user!
Dan.